Transcript
00:00Thank you for joining us today on our Burnie Quick tap installation video.
00:05Today we will be installing the burnie thermal weld quick tap,
00:08first drive the ground rod into the earth with around 3 ft of the ground rod staying above
00:14grade.
00:26Next, make a mark at least an inch from the top of the ground rod.
00:31This is how far down the quick tap coupling should be compressed.
00:35Ensuring a safe connection, remove the caps
00:42and place the coupling onto the ground rod and tap with a hammer so that it is fitted and
00:47ready for installation.
00:49Drive the quick tap until the coupling completely crosses the line that was marked
00:54about one inch from the top finish driving the ground rod.
01:03The Quick tap can be utilized in a variety of applications including commercial
01:09residential
01:17and even fence post connections.
01:26Part two to make a connection using two quick taps, use a drive sleeve to align them properly
01:33to prepare for the ground rod installation.
01:37Remove the cap and place the first quick tap over the drive sleeve,
01:50remove the cap of the second one and place it on top of the first one.
01:55For this example. We have two wires coming to the ground rod.
01:59The drive sleeve will help us line up the two couplings exactly the way we want them.
02:04Before making the permanent connection, tap the quick tap with a hammer to secure it to the
02:11ground rod complete the
02:18connection by driving the two couplings together.
02:20Using the same method you would use to drive a ground rod.
02:24You will know the connection is complete. When the two couplings are entirely in contact
02:29with each other, the double quick tap connection will be connected to ground rod
02:34using the same instructions as a single quick tap.