text.skipToContent text.skipToNavigation

 

SpectraClean Estimator Banner

Spectraclean App Bullet Points Column 1
Spectraclean App Bullet Points Column 2
Web Browser
Web Browser
Mobile App
Mobile App

Estimator Tool Terms and Conditions


The Estimator Tool may only be used to provide preliminary estimates for luminaire quantity, placement and operation time. It should not be relied upon to determine the actual maximum operation time or min/max dosing time range. It is the responsibility of the installer to determine the maximum operation time, min/max dosing time range, and maximum irradiance values using field measurements for the specific application per International Electrotechnical Commission (IEC) 62471 acceptable risk groups and American Conference of Governmental Industrial Hygienists (ACGIH) Threshold Limit Value (TLV). An installer should conduct a post-commissioning operation audit of irradiance levels in the space before a room is occupied. Hubbell is not responsible for ensuring that occupants of the space will not be exposed to excessive UV or optical radiation during equipment operation.