Project Profiles

Zipcar
The unique shape of the Sector M5 completes the design of Zipcar's new headquarters located in Boston. see details

Susitna Valley Jr./Sr. High School
This LEED Silver certified high school in Talkeetna, Alaska experiences precious few daylight hours during the winter months which means energy efficient lighting was a key element in its design. see details

Litecontrol Headquarters
Litecontrol"s headquarters underwent a major renovation between 2012 and 2013. see details

Open office and conference room
This downtown Chicago office was completely renovated in spring of 2011. The space uses the 82M from the Latitude line in the open office spaces. The 82M is also used in tandem with the Wall/Wash 4400 in the agency’s conference rooms. see details

Cooper University Hospital Patient Care Pavilion
Winner of the 2008 New Jersey Smart Growth award and the 2010 Award for Merit for Interior Lighting from the Illuminating Engineering Society North America, Philadelphia Section. see details

Federal Center South, Seattle WA
The newly renovated home of the U.S. Army Corps of Engineers, Seattle District not only enjoys views of the Duwamish Waterway but also houses an office full of pendant indirect/direct "dead special" fixtures. see details

Geisinger Health System - Hood Center for Health Research
The newest addition to Geisinger Health System, Center for Health Research facility, is a 68,000 sf facility and links the Weis Research Facility with the main campus. see details

Jackson Hole Airport
In 2011, The Jackson Hole Airport was expanded and renovated to reflect it's surroundings, Wyoming's Grand Tetons. Litecontrol's Mod 44 pendant with staggered lamps hang above the ticket agents while Mod 46 Wall mounted fixtures and Recessed Mod 44 fixtures are installed in the concourse and common areas.

William Oxley Thompson Memorial Library at OSU
The Staklite 500 graces the recently renovated William Oxley Thompson Memorial Library. The library has undergone three renovations/expansions since it was originally opened on January 6, 1913. see details

SPiN Milwaukee
What better way to light up your table tennis match than with the pendant Mod 22 Direct? Spin Milwaukee is a table tennis club that features 12 tables and one center court as well as a bar, restaurant and pro shop. see details

ShopRite, Hatfield, PA
The SDx with the High Performance Baffle graces the checkout lanes in this Hatfield, PA ShopRite grocery store. see details

SHI International
In this project, the Mod 66 TechZone with dimming ballast transforms a conference room into a versatile multipurpose room, while the clean lines of the Aura add elegance to the fitness room. see details

ShopRite, Tom's River, NJ
The Wall SAE illuminates more than groceries in the Tom's River, NJ ShopRite. These fixtures were chosen because the owner needed efficient lighting to boost up onto a mural that graces the store's walls. see details

IHG Atlanta, GA
The Arcos Perf and Mod 46 Pendant brighten up this vibrant Atlanta-based headquarters. Open office spaces are illuminated by the diffuse light of the Arcos Perf Indirect luminaire, while the Mod 46 I/D lights up the common areas. see details

John Spoor Broome Library
The John Spoor Broome Library is located on the California State University, Channel Islands (CSUCI) campus in Camarillo, California. The library formally opened on April 4, 2008 and was named a winner in the California Construction magazine Best of 2008 awards program. The Library won the Award of Merit in the Outstanding Architectural Design category. An independent jury of industry experts in design and construction judged more than 140 nominated projects in a variety of categories see details

Nixon Art Associates, Inc.
Based in downtown Chicago, Nixon Art Associates offers a full range of curatorial services. The firm specializes in art acquisition, documentation, framing, installation, liquidation, valuation, restoration, appraisal, exhibition and archiving. see details

WMU Chemistry Building
The Western Michigan University Chemistry Building in Kalamazoo utilizes daylighting controls which automatically dim and switch off fixtures when natural light levels allow. see details

USBGC Headquarters
In 2009, The US Green Building Council's Washington, DC based headquarters became the first space to achieve LEED Platinum under the Commercial Interiors (CI) rating system. Litecontrol played a large part in this success by providing high efficiency/low energy lighting to the project. see details

Africana Studies and Research Center, Cornell University
Completed in 2005, the award-winning Africana Studies and Research Center measures 11,600 square feet with two pavilions, totaling 6,000 square feet. see details

Pete's Fresh Market
This family owned and operated supermarket chain in the Greater Chicago area prides itself on only selling quality product. The owners have high regard for architecture and strive to give their customers a comfortable atmosphere in which to shop. So it was no surprise that they asked Litecontrol to light their Calumet and Evergreen stores. see details

Homewood Middle School
Completed in January 2005, Homewood Middle School was the first middle school in the nation to be rated LEED Silver. The building replaced a 50 year old school that proved too costly to renovate. see details

Richmond International Airport
Dedicated in July 2007, the construction of the Richmond International Airport terminal included concourse expansions and renovations, new and expanded parking structures, new signage and wayfinding. The building included 160,000 square feet of ticketing, baggage claim and concessions space. The multi-award winning Richmond International Airport, boasts many Litecontrol fixtures. Litecontrol product V3 see details

Alberici Corporate Headquarters
Completed in December 2004, the new headquarters for one of St. Louis' oldest and largest construction companies adapted and repurposed an existing manufacturing plant. see details

Bismarck Airport
Construction of the new Bismarck Airport terminal was completed in the spring of 2005. The new 70,000 square foot terminal building is 57 feet tall with sky painted vaulted ceilings, a geo-thermal heating and cooling system, and a state of the art baggage handling system. see details

Lakeside Trainers Club
The Lakeside Trainers Club was originally an office space that was converted to a 9,000 square foot fitness center by Kenny & Khan Inc. Architects. see details

Lone Mountain Elementary School
Lone Mountain Elementary School is a perfect example of how effective efficient, pendant classroom lighting can be. see details