text.skipToContent text.skipToNavigation

Bismarck Airport

Bismarck, ND

Construction of the new Bismarck Airport terminal was completed in the spring of 2005. The new 70,000 square foot terminal building is 57 feet tall with sky painted vaulted ceilings, a geo-thermal heating and cooling system, and a state of the art baggage handling system. Other amenities include a restaurant with beer and wine service, business kiosks with plug-in internet access, and wireless internet. The new building is located just northwest of the old passenger terminal, which was demolished after moving into the new building.