text.skipToContent text.skipToNavigation

Pete's Fresh Market

This family owned and operated supermarket chain in the Greater Chicago area prides itself on only selling quality product. The owners have high regard for architecture and strive to give their customers a comfortable atmosphere in which to shop. So it was no surprise that they asked Litecontrol to light their Calumet and Evergreen stores.

The challenge was to provide a luminaire that could distribute high footcandle levels from top to bottom of product shelving with even light distribution, using mostly direct lighting. The luminaire also needed to reflect the upscale, modern look of the store. The SDx with green acrylic baffles and 2-T5HO lamps was chosen for its great aesthetics, performance and efficiency. Also installed in the project are surface-mounted Mod 44 direct.

Litecontrol product

SDx

Arcos 5900

Mod 44 direct