text.skipToContent text.skipToNavigation

energy efficiency,  Outdoor Lighting,  Progress Lighting

5 tips to extend the outdoor living season

The prevalence and popularity of outdoor living comforts are on the rise, as homeowners become accustomed to the many benefits exterior spaces have to offer. With cooler and shorter days just around the corner, now is the time to start preparing the outdoor spaces of your home for relaxing and entertaining that will transcend the seasons. Don’t let the darkness chase you indoors; with the right tools and techniques, you can extend your outdoor living season all year round.

6 Ideas for Better Outdoor Living

Make your outdoor areas more enjoyable and “livable” – from season to season with these 5 tips!

  1. Illuminating your living spaces keeps your home’s exterior welcoming and comfortable. Areas that are frequently used after nightfall, such as a deck or patio, should be appropriately lit with fixtures that complement the structure. Choose fixtures that further the unique architectural elements of your home. Decorative post, hanging and wall lanterns can be easily installed to brighten your outdoor areas.
  2. LED lighting is a highly energy efficient solution that offers many benefits for outdoor living. Not only can installing LED fixtures lower your energy bill, but also the longevity of LED technology makes them a very low-maintenance addition. No need to go through the hassle of changing bulbs when these sources last for decades. Plus, improved color temperature options provide a nice warm, inviting glow to illuminate outdoor living areas.
  3. Brighten your pathways with landscape lights to improve safety and security. Path lights can also make your yard visually appear larger. Position lights on alternate sides for even illumination. Avoid shadows when used at steps, as well as away from plants so they don’t interfere with light distribution.
  4. Use accent lighting techniques to highlight entryways and stationary pieces to create points of interest. These focal points will engage visitors and encourage them to take a closer look.
  5. Remember to show balance and symmetry in your lighting design. Lighting should be proportional across the various areas of the property. Highlight symmetrical components in different landscape areas, such as columns or corresponding bushes. The goal is for the amount of illumination within and across different areas to be symmetrical.