text.skipToContent text.skipToNavigation

lighting designs

Easy Lighting Hacks to Reduce Glare

Oh, my aching head! If you’ve recently started working at home, some of the things you take for granted in your workplace may be issues at home. At work, it was easy to call maintenance or put in a request for service if you needed new batteries or a fresh light bulb. At home, guess what? You are the maintenance person.

Working at home is new to a lot of us! As we posted in an earlier blog, proper lighting is key to setting up a productive workspace. Visual discomfort tops the list of pain-causing, work-at-home woes. Let’s talk about glare, which is probably the most common cause of daily headaches and blurred vision.

Equinox Collection | Image: Toll Brothers

What exactly is glare?
There are two types of glare: discomfort glare and disability glare. Discomfort glare happens when light is too direct or reflects too strongly off a surface, creating a bright, dazzling light. Direct light from overhead fixtures or sun streaming in from a window bounces off your desk or computer screen and into your eyes, causing the pupil to constrict, allowing less light in. As the day progresses, your eyes are continually adapting to changing light levels, and that’s what causes those killer headaches and eye fatigue.

Disability glare reduces how well we can see. Disability glare can be caused by eye conditions, like cataracts, and can occur with conventional light sources and levels of light. Disability glare reduces contrast, making it difficult to see details or distinguish objects. This type of light sensitivity usually requires medical treatment, but there are also ways that lighting can be adjusted to alleviate discomfort from glare.

Cinq Collection | Image: Schumacher Homes and Possibilities For Design

Regardless of which type of glare you’re experiencing, lighting can help! Here are some easy lighting hacks to solve the problem of glare.

  1. Use indirect lighting that throws more light upward than downward, diffusing the light and reducing glare on computer screens and work surfaces.
  2. Relocate the light source behind, or perpendicular to the computer workstation so that light is not shining directly on the computer monitor.
  3. Change position. Try relocating the task to another area or change its orientation until the glare goes away.
  4. Use blinds or shades on windows to control the amount or angle of sunlight entering the room.
  5. Use dedicated task lighting for activities such as reading. Position the light below your eye level and between you and the object for the best visibility.

We hope these tips make your #StayatHome time as comfortable and productive as possible. Take care.

Looking for more design guidance and inspiration? Visit our Style section.