text.skipToContent text.skipToNavigation

Progress Lighting,  Uncategorized

Martha Childress Fundraising Opportunities

The HBA of Greenville Board of Directors has formed the Martha Childress Task Force to modify Martha’s home in preparation for returning from a rehabilitation facility. Martha continues to heal and is making great strides in recovering from a gunshot wound that left her paralyzed from the waist down.

Progress Lighting is proud to be part of the HBA community that is helping to make a difference for the Childress family. Please consider supporting this initiative.

If you are unable to contribute labor or materials to these two projects, please consider a cash contribution to the Martha Childress Housing Fund. All proceeds not spent on her housing needs will be donated to a fund for her ongoing health needs. Checks can be made payable to HBA of Greenville Attn: Martha Childress Fund, 5 Creekside Park Court Ste. A, Greenville, SC 29615.

Additional fundraising opportunities have been set up to help Martha (http://elephantstrong.org/fundraising.html).

If you have any questions, please contact the HBA office at info@hbaofgreenville.com or (864) 254-0133.

Original source: http://hbaofgreenville.blogspot.com/2013/11/martha-childress-task-force-and.html