Sneak Peek! New Exterior Lighting from Jeffrey Alan Marks

Progress Lighting gives a sneak peek of designer Jeffrey Alan Marks Point Dume Collection new exterior lighting fixtures for homes from coast to coast.

We're excited to announce the debut of designer Jeffrey Alan Mark's Point Dume™ Exterior Collection as part of our Design Series lighting line. The new exterior collection joins the well-received Point Dume™ Collection of interior lighting by Jeffrey Alan Marks, which enters its third year of collaboration with Progress Lighting.

"Outdoor lighting is incredibly important to me", states Jeffrey Alan Marks, "Outdoor lighting establishes the entry of a home and of course entertaining outside has become even more important to all of us. I have expanded many clients living spaces to the outdoors and my collection is the perfect way to illuminate these exterior rooms. I designed the collection with Progress Lighting using materials like corrugated metal which reflect an East coast feeling typically seen on barns. From hanging lanterns to chandeliers there is a style for everyone."

The Point Dume™ Exterior Collection features six new family designs, encompassing 31 styles of hanging lanterns, wall lanterns, LED sconces and pendants. Here's a sneak peek of the new Jeffrey Alan Marks fixtures.

HOOK POND
Evoking thoughts of Jeffrey's East Coast summer home, the Hook Pond Collection features a steeply pitched, barn-inspired roof crowned with a distinctive loop finial. A clean, modern frame holds glass panels printed with a unique silver mesh pattern reminiscent of a traditional screened-in porch. Light is comfortably diffused from the white opal glass orb held within the generously scaled frame.

Hook Pond wall lanterns are made with DURASHIELD, a durable material specially designed and tested to resist harsh environmental conditions. A choice of three Finishes: soft Oil Rubbed Bronze, contemporary Shelter White, and a classic Galvanized metal.

SEAMOOR
For Seamoor, Jeffrey created a sophisticated adaptation of the utilitarian metal roofs found on barns throughout the countryside. A square frame supports a wavy roof inspired by traditional corrugated rooflines. The rectangular handle is reminiscent of handles on old barn lanterns, but its oversized scale adds a contemporary element. Clear glass panels surround a classic silver reflector on the back panel, enhancing the glow cast from an elegant double candle holder.

Made with DURASHIELD, a durable material specially designed and tested to resist harshenvironmental conditions. A choice of two finishes: soft Oil Rubbed Bronze, classic Galvanized metal make Seamoor perfectly at home in locations from coast to coast.


WAKECREST LED
The Wakecrest LED Wall Sconce is a contemporary take on rustic luxury. Jeffrey translated the corrugated rooflines of classic barns into a softly waved sconce frame, paying homage to the Americana aesthetic. A crisp, sharp edge defines the modern roof peak and complements the vintage character of the fixture's design.

Made with DURASHIELD, a durable material specially designed and tested to resist harshenvironmental conditions. LED lamping offers energy-efficient, long-lasting light for outdoor spaces. Three finish options include the crisp Shelter White, modern Matte Black, and classic Galvanized —and two wall fixture sizes deliver design flexibility suitable for homes across the nation.


EDGECLIFF
The Edgecliff Pendant celebrates the austere simplicity and functionality of America's architecturally distinct corrugated metal-clad buildings. Crisp, sharp lines form a frame of iconic metal curves, making a sculptural gesture to its traditional inspiration. Silver mesh patterned glass on each end of the frame provides a luxurious touch to the rustic design. Jeffrey recommends using exposed filament style bulbs in the open-bottom frame to further the authentic Farmhouse style of the light. Edgecliff is offered in a contemporary Shelter White, a classic Oil Rubbed Bronze and smooth Galvanized finish choices, continuing the Americana inspiration of the pendant.

DUNEMERE
Homes from coast to coast will appreciate how the Dunemere Wall Lantern embodies Jeffrey's love of casual, relaxed outdoor living. Vintage barn details of symmetrical gables and a slanted corrugated roof form a peaked canopy over modern ribbed lamp holders and clear glass panels .Made with DURASHIELD, a durable material specially designed and tested to resist harsh environmental conditions

A clean Shelter White finish creates a contemporary style choice for Dunemere, while modern Matte Black and classic Galvanized offer a more timeless selection for its iconic, barn-like silhouette. Jeffrey created Dunemere in three sizes to complement a range of relaxed, outdoor living spaces from coast to coast.

SHADMORE
With the Shadmore Pendant, Jeffrey embraces bold architectural influences to create a minimalistic design that effectively blurs the lines between indoor and outdoor living. Airy interconnected geometric cubes form a spacious frame giving the light a modern personality. An elegant, marbleized acrylic shade creates a striking focal point while delivering an inviting, warm glow. Shadmore is available in a crisp Galvanized or modern Matte Black finish combined with a smooth White Marble center shade.

The new Point Dume™ exterior fixtures will be available at lighting showrooms, online retailers, and on our website, www.progresslighting.com, in January 2022.