Product Announcement
Seismic Certified Transformers for Critical Infrastructure

Ensuring the resilience of infrastructure during and after earthquakes is vital, especially for critical facilities including hospitals, fire stations and government buildings. Seismic qualification guarantees essential components, such as transformers, can withstand seismic events and remain operational.
ACME is proud to introduce our line of seismic certified transformers. The initial launch includes three phase ventilated products 15 to 500 kVA. Designed specifically for the commercial construction market, they will allow our distributors to sell into markets that require seismic certification. Particular focus will be to support first responders on the west coast and other seismically active regions.
ACME’s transformers have undergone rigorous testing to meet the International Building Code (IBC 2015) and California Building Code (CBC 2016) standards. Each product is certified in accordance with ICC-ES AC156 seismic qualifications, verifying its ability to endure and perform under extreme conditions.
Learn more about ACME products by visiting https://www.hubbell.com/acmeelectric/en