Transcript
00:02Welcome to Acme Electric Transformer seminar. In this session,
00:06we will be discussing K factor transformers, harmonic mitigating transformers and I trap
00:12neutral current reducer harmonics are a
00:19sinusoidal waveform with a frequency that is an integral multiple of the fundamental frequency.
00:24For instance, if 60 Hertz is the fundamental frequency, then 120 Hertz would be the second
00:30harmonic. 180 Hertz would be the third harmonic and so
00:34forth. Both the
00:41fundamental 60 Hertz and the fifth harmonic 300 Hertz are purely sinusoidal.
00:47All harmonic frequencies are sinusoidal. When viewed individually in the next slide,
00:53we will see that they can appear as complex or distorted waves when viewed simultaneously.
01:03Here we see a typical wave form of fundamental and fifth harmonic together notice the
01:08distorted or non linear shape
01:16harmonics primarily originate in electronic power converters.
01:20These can be found in switch mode, power supplies electronic ballasts,
01:26variable frequency drives oven and furnace controls and rectifier circuits.
01:32Harmonics originate any time current is being drawn in short rapid pulses rather than in a
01:37smooth continuous manner.
01:44Some of the problems that can be created by harmonic occurrences are overheated,
01:49neutrals, overheated transformers, malfunctioning of equipment due to excessive
01:55voltage distortion, burned out motors, tripped circuit breakers and blown
02:02fuses. It should be noted that a major side effect of
02:05harmonics is extra heating in all system components.
02:12Triple harmonics include the third harmonic and all the odd multiples of the third.
02:18For example, the 3rd, 9th, 15th, 21st, 27th, 33rd and
02:25so forth. It should be noted that triple harmonics tend
02:29to add up in the three phase neutral conductor,
02:3760 Hertz or fundamental currents tend to cancel in the three phase neutral because of the 120
02:43degree phase shift between adjacent phases.
02:46Triple harmonics add up in the three phase neutral because they are in phase with each
02:51other. The effects of harmonics on transformers
02:58include increased temperature rise, increased neutral current flow,
03:04increased core losses, increased sound level and decreased efficiency,
03:11stray losses in the conductors get multiplied by the K factor of the load to increase winding
03:16rise. Triple harmonic currents add up in the three
03:19phase neutral harmonic voltages tend to increase losses in the iron core.
03:28The K factor is a mathematical formula for calculating the heating effects of harmonics.
03:34It is a measure of a transformer's ability to withstand the heating effects of non sinusoidal
03:40harmonic currents created by much of today's electronic equipment.
03:44The stray losses of the transformer are multiplied by the K factor of the load
03:49resulting in increased heating of the unit.
03:56Next, we will discuss transformer conductor losses transformer conductor losses are
04:02composed of AC and DC losses.
04:05AC losses, equal stray losses.
04:08DC losses, equal I squared R total conductor losses, equal AC plus DC
04:15losses, I squared R losses can be easily determined from current and resistance.
04:20Stray losses are more difficult. Transformer. Total losses can be measured by putting a watt
04:26meter in the primary supply circuit.
04:28The I squared R losses can be subtracted from this total and the remainder would be the stray
04:33losses. In this example, we see a
04:40standard distribution 75 K VA transformer has 2995 watts of total
04:47conductor losses at K one assuming a linear load.
04:51However, if the load would not be linear, for example, at K 20 the new losses would be
04:575560 watts.
05:00This would increase the transformer temperature rise from 150 °C to 244
05:06degrees resulting in overheating, shortened the transformer lifespan and possible cause for
05:12failure. There are three solutions to
05:18harmonic problems.
05:20K rated transformers, harmonic mitigating transformers, an eye trap neutral current
05:27reducer. First, we will discuss K RD
05:34transformers, K rated or nonlinear transformers do not eliminate harmonics.
05:40They are only designed to tolerate the heating effects of harmonics created by much of today's
05:45electronic equipment.
05:51K RD transformers are traditional Delta Y transformers.
05:55They are designed with lower flux densities and no load losses as well as lower I squared R
06:01losses resulting in a larger and heavier unit.
06:04They do not eliminate or cancel harmonics.
06:11K factor features include being available in K factors of 413 and 20.
06:19They are available with aluminum or copper windings.
06:23They have temperature rises of 1 51 15 or 80 and they are listed and CSA
06:29certified as of January 1st
06:362016. Kr Transformers must comply to the efficiency
06:40standards. Doe 2016 of the National Energy Bill.
06:46They are only required to comply with a connected load condition of K one no harmonics.
06:56Next, we will discuss harmonic mitigating transformers.
06:59They consist of a delta primary and a zigzag secondary.
07:04The zigzag secondary causes a phase shift in the triple harmonics which results in a
07:09canceling effect.
07:10This prevents the triple harmonic losses from being coupled back into the primary and results
07:16in cooler operation and increased energy efficiency.
07:23Let's discuss what a zigzag winding is the secondary winding on each magnetic leg of the
07:29core is wound in two separate sections. These sections are then transposed between
07:34different legs of the core to create the zig zag secondary.
07:39Each 120 volt output of the transformer consists of two sections from different
07:44magnetic legs resulting in a magnetic phase shift.
07:52Here we see a diagram that shows the delta primary and the zigzag secondary.
08:01There are several benefits to harmonic mitigating transformers.
08:05Unlike K rated transformers, harmonic mitigating transformers actually treat the
08:10triple and harmonics in the zig zag secondary winding, they reduce supply voltage flat
08:15topping caused by nonlinear loads.
08:18They improve overall power factor of supply systems.
08:22They are suitable for K factor loads and they provide improved energy efficiency which meets
08:28the doe 2016 at K one load
08:36mitigating transformer features include copper foil conductor to minimize skin effect of
08:42harmonic currents. Two taps at 2.5% above and below nominal
08:48220 °C insulation system with 150 °C rise, UL listed and
08:55CSA certified and zero degree angular displacement between primary and secondary
09:01windings. Harmonic mitigating transformers
09:08don't treat harmonics or neutral current until they reach the transformer windings.
09:12Harmonic mitigating transformers has 200% neutral bar neutral conductor from the
09:18transformer to load panel should be sized at 200%.
09:26Acne transformers have definitive advantages.
09:29Acne utilizes special winding techniques and foil conductors in both its K factor and
09:34harmonic mitigating transformers to minimize the heating effects of harmonic currents.
09:39The use of foil conductor increases the dielectric strength of the insulation because
09:44one layer is only one turn foil also eliminates the effects of axial forces which can result in
09:51failure of wire wound transformers.
09:58Next, we'll discuss skin effect.
10:00Skin effect is directly proportional to the height or thickness of the conductor.
10:05Some manufacturers use parallel strands of thinner wire to reduce skin effect,
10:09but acne uses foil conductors to get maximum reduction of skin effect
10:17applications that use harmonic mitigating transformers are hospitals and health care
10:22facilities, commercial and educational facilities, airport facilities,
10:28telecom facilities, broadcasting facilities, internet service providers and data
10:34centers. Next, we'll
10:41discuss an eye trap neutral current reducer.
10:45The technical description of an eye trap neutral current reducer is that it is low
10:49impedance zero sequence and is an auto zigzag transformer.
10:58Some applications of an eye trap neutral current reducer are it is used to reduce
11:03excessive current flow in the neutral of a three phase 208 delta 120 volt system.
11:10It is available in AMP ratings of 101 153 104 150.
11:16It includes a front mounted amp meter for monitoring.
11:19Neutral current target areas include data processing centers,
11:24hospitals, radio and TV stations, large computer labs and so forth.
11:29Any area having numerous electronic 120 volt loads powered from a 208 delta 120
11:36system. How does the eye trap
11:42work? The third harmonic currents are in phase in the
11:47three phase neutral.
11:49The low impedance and auto zig zag characteristics of the eye trap target.
11:53The third harmonic currents causing them to become out of phase in the three phase neutral
11:58resulting in a canceling effect reductions of 50% to 90% are typical in many
12:05applications. The ACME Irep provides an easier and more
12:08affordable solution than replacing existing neutral conductors.
12:16Eye TRP helps reduce unbalance in the phases which helps reduce neutral current.
12:21As we see here in this slide, the eye
12:28trap is not a harmonic filter, but it does tend to reduce total harmonic distortion in the
12:32phases. It also slightly reduces the K factor of the
12:36system which allows the supply transformer to operate a little cooler,
12:40resulting in longer life. If this transformer is ever replaced,
12:44we recommend that it be replaced with a K factor unit.
12:51Here we see that the total neutral current of 84.8 is greater than the highest phase current
12:57of 63.2.
12:59Notice that the total neutral current has been reduced by almost 90% 84.8 to 8.1
13:06amps. If you have questions about any of the
13:13transformers discussed in today's session, call us at 1 803
13:18345214 or you can email our tech group at PDPD tech support at
13:25Hubble acme.com.