text.skipToContent text.skipToNavigation

2016,  News,  Progress Lighting

Progress Lighting unveils new collections in line with industry trends

  • Hand-crafted elements. Industrial influences. Mixed metallic tones. The lighting trend report is in! At Progress Lighting, we are dedicated to providing high quality lighting solutions that complement and enhance the latest looks in home fashion. And we feel our 2016 introductions do just that. If you’ve been following along on our Facebook and Instagram pages, you’ve seen peeks into our new families. Now, we are ready to give you the full reveal!
  • We have an exciting week planned as we head to Texas for the inaugural Lightovation show at Dallas Market – and simultaneously exhibit at the International Builders’ Show in Vegas. At both shows, we are unveiling our 2016 introductions, which include nearly 30 new collections and 17 collection expansions. Among these new families are energy efficient LED lines, on-trend interior fixtures and outdoor lighting designed to beautify the exterior of the home. Enjoy some of the highlights below!
  • Mixed metals, vintage undertones.

Swing introductions

  • Collection Expansion: Swing
  • The Swing collection, unveiled in January 2015, has grown to include spheres and pendants that mimic the authentic, industrial style of the family’s original linear and round, warehouse-styled fixture designs. Exposed Edison bulbs provide added visual appeal, while mixed metal accents embrace the popular trend to vary finishes within one space.
  • Lighting as art.

Indi

  • New collection: Indi
  • Slightly larger in scale than a traditional pendant, these fixtures are artistically styled and can be clustered to fill spacious interior areas. Antique mirrored glass shine through when illuminated. The Indi family plays into the trend for lighting fixtures to serve as captivating focal points of a room.

 

  • Vintage design styling.

Lucky collection

  • Collection expansion: Lucky

 

  • The popularity of the Lucky bath and vanity fixtures fueled the decision to grow this loved series of vintage inspired fixtures. Light is beautifully illuminated through soft prismatic glass. Precise details in the tubing, frame and shades enhance the vintage design styling. New fixture options are available to illuminate kitchens, bedrooms, hallways and living areas.

 

  • Creative in spirit. Crafted with care.

Cirrine

  • New collection: Cirrine

 

  • Cirrine appeals to the creative spirit within all of us. Hand formed arching elements are highlighted by an artistic painted finish the feathers from a rich bronze tone to a vintage brass accent. Etched white glass complements the artistic frame. With its hand crafted nature, Cirrine furthers the trend of “lighting as art.”
  • Now trending: Casual Luxe.

Esteem

  • New collection: Esteem

 

  • Esteem’s exaggerated classic frame offers casual luxe styling for the home. Oversized single tiered chandeliers with K9 finial accents. The foyer pendant features a frameless design to suspend glass panels, creating a floating effect for this elegant fixture.

 

  • Pleasingly retro. Updated in efficiency.
  • Pure LEDNew collection: Pure

 

  • Pendant applications with LED module features designer oriented details in the new Pure collection. Available in several finish options, including Brushed Nickel, White or Antique Bronze with anodized gold inside, as well as retro Pistachio Green. The collection offers a retro vibe – but is updated with a modern LED source. 623 lumens, 90+ CRI, 3000K color temperature.