Solutions OverviewBenefits are derived from well implemented Solutions. The challenge to save energy, improve safety or make sure everything continues to perform in a harsh environment, are all candidates for good solutions.
Markets OverviewHubbell serves the needs of customers in a variety of market applications. See our major markets and building types below.
Transcript
00:00Today, we're going to demonstrate how to install and use the MM410 weatherproof.
00:05While in-use device covered, the unit comes with a cover base,
00:10mounting screws and two adapter plates if needed.
00:16The adapters snap in from the backside of the base which is the side with the attached gasket.
00:22We're installing this vertically.
00:24So using a player will remove the single cord port on the bottom side.
00:29If this was a horizontal installation, the ports on the wider side would be removed.
00:33Instead of course, as with any electrical work, make sure the power is off at the breaker start
00:39by backing out device, mounting screws about a half inch if installing on a rough surface.
00:44Apply a quarter inch bead of silicone caulk between the base and wall surface align key
00:50holes on the base with screws slide over base and fasten screws.
00:58Compress gasket by tightening screws until snug.
01:02All that is left is to attach the cover, align hinge pins on base with holes on cover and push
01:08sideways to snap in place to allow the hinges to line up properly.
01:13Angle the cover between 60 and 80 degrees before snapping together. Installation is complete.
01:22Your MM410 cover is now ready for use.