Transcript
00:09Hubbell TAYMAC has added a unique solution to our market leading weatherproof device cover line
00:13with the MR420, a recessed wall outlet enclosure kit.
00:17The national electric code requires device covers in wet locations to be weatherproof
00:22while in use or not. A bubble cover is a typical code compliant
00:26choice. While this is fine for many installs, a bubble
00:30cover simply may not cut it where space or aesthetics are important.
00:34The MR420 solves any issues where a bubble cover just won't cut it.
00:38It is also an excellent choice for many standard installations due to the compact all
00:43in one clean design.
00:45The innovative design is made up of three main components starting with an optional siding,
00:50flange, a recessed electrical box and the cover assembly that all nest together creating a
00:55weatherproof seal.
00:57Since the cover and receptacle are recessed inside the electrical box,
01:02the cover doesn't protrude into the surrounding space even with a cord plugged in for
01:06continuous use.
01:07This meets the latest NEC requirements including extra duty.
01:12The MR420 comes ready to install on almost any wall surface.
01:15It's available in three color options, all with a clear cover and it's paint too to match the
01:19surrounding wall. I'm going to walk you through a couple of
01:21common installations as with any electrical work.
01:24Make sure the power is off at the breaker.
01:28The first step is choosing the location.
01:30Make sure all building and electrical codes will be satisfied before making any cuts in the
01:34wall. I've located the nearest wall stud to mount the
01:37electrical box. If I was sure that a layer of plywood existed
01:40behind the stucco, I could mount anywhere I wanted. The siding flange isn't needed in a
01:44typical stucco wall, but it makes an excellent template for the cut in.
01:48I'm marking the inside of the template. So make sure you cut a bit outside of the line.
01:52If I was upgrading an existing outlet, I'd need to remove the device and box and enlarge the
01:57hole. The original box is most likely against the
02:00stud already. Once the hole is cut, I'll fish my wires,
02:03making sure to follow all national and local codes. Knockouts are available if I was using
02:08Conduit, but I'm running Romex.
02:10So I'll stab through one of the included cable clamps in the electrical box.
02:14Make sure to leave enough wire to properly wire the device after mounting the box.
02:18Now I'm ready to mount the electrical box. Due to the uneven surface,
02:22it's recommended to run a quarter inch bead of non hardening silicone cad.
02:26The box can now be maneuvered into the opening and mounted to the stud with the two included
02:30lag screws. If this was a horizontal install,
02:34I'd use the alternate screw mounting holes.
02:38Now I'm ready to install the device. Since we're outdoors,
02:41I'm using a GFC. If we were on a GFC protected circuit already,
02:45I could use a duplex by simply swapping out the adapter in the back of the box.
02:49A single round adapter is also included.
02:52The cover is now ready to be mounted in place. There's no cork necessary on this gasket.
03:00Simply drive the two mounting screws until the cover is completely seated.
03:04Turn the power back on and that's it.
03:06Installing on other wall types is just as easy.
03:09If I were installing on vinyl siding, I'd simply screw or nail the siding flange in the
03:13desired location like I've done in the display board here.
03:16This works for new construction when the sheeting is exposed or for remodel projects by
03:21simply removing some siding first instead of mounting to the framing with the included L
03:25screws. I can mount directly to the siding flange with
03:28the four included screws. For a new brick or block wall installation,
03:32install the electrical box in a bed of mortar. While the wall is being constructed.
03:36If upgrading an existing outlet in a brick or block wall,
03:39remove the device and box and enlarge the hole like we did on the Stucco wall,
03:43it's always a good idea to run proper anchoring screws through the front face to hold the box
03:48in place. I'd also anchor the flange with the same screws
03:50on a new work brick or block wall while the mortar is curing.
03:53We've included a place on the package for project number or name.
03:57This is especially handy if you need to store the cover assembly for prolonged periods during
04:01the construction project.
04:04There are alternate holes for any cover mounting preference.
04:10The rest of the install follows the same procedure.
04:12I've showed you earlier and there you have it. The MR420 is a code compliant innovative
04:17solution where either space or appearance are deciding factors.
04:22So for any of your outdoor electrical needs, look to Hubbell TAYMAC and Bell for proven and
04:27innovative weatherproof solutions.