Product Announcement
Byant Electric Announces New USB Switch Combination Charger
Bryant Electric is excited to announce its new USB Switch Combination Charger device, which features two-port USB charging along with a 15 Amp switch. This innovative device works in a single-gang opening to allow placement of USB charging capability in locations typically reserved for switches, such as near countertops, desktops, or vanity areas. Installed in place of a traditional switch, the USB Switch Combination Charger device allows users to control lights or receptacles while also providing a convenient place to power electronics via USB. The switch is capable of single-pole or three-way wiring to accommodate control from two points; the switch is isolated from the USB for independent use. Providing 2.1 amps of charging power, the device can safely charge: • Smartphones • Tablets • Laptops • MP3 players • Digital cameras • Other electronic devices "With numerous electronic devices now found in almost every home, Bryant's new USB Switch Combination Charger device allows homeowners to add charging capability without taking up more wall space," says Vic Flagello, director of residential marketing for Bryant Electric. "When placed near surfaces, these devices help establish ‚Äòdrop zones' that maximize space while providing a convenient place to power electronics." The devices are suitable for new construction or renovation projects, and are available in six colors - brown, ivory, white, gray, black, and light almond - to match any home's decor. For more information about Bryant's New USB Switch Combination Charger device, or any of their other industrial, commercial, or residential products, contact your Bryant sales representative, Bryant customer service at 1-800-323-2792, or visit www.bryant-electric.com.