Transcript
00:04Introducing Bryant's expanded line of occupancy and vacancy sensors utilizing advanced
00:10technology for maximum performance.
00:12Bryant offers a complete line of occupancy and vacancy sensors including wall switches,
00:17wall mounted sensors and ceiling sensors designed for a broad range of applications in
00:22both commercial and residential settings, such as offices,
00:25hallways, lobbies, classrooms, large gathering areas, restrooms,
00:30small closets, pantries anywhere there's opportunity for energy savings.
00:35Bryant features the latest technological advances including its breakthrough adaptive
00:40technology and its dual technology, motion sensors that use both passive infrared and
00:46ultrasonic technologies together for maximum coverage and flexibility.
00:50These sensors are a perfect solution for reduced energy costs,
00:54fewer adjustments and less maintenance.
00:59Adaptive technology is a Bryant patented breakthrough that delivers a true install and
01:04forget operation.
01:05Adaptive technology sensors use microprocessor technology that constantly monitors the area
01:11and automatically adjusts the sensitivity and timer based on activity.
01:15It literally fingerprints movements, motion patterns and occupancy habits then modify
01:21settings to eliminate occupant disturbance. While maximizing savings.
01:25By choosing adaptive technology sensors, you no longer have to make manual adjustments for
01:30furniture layouts, seasonal changes or occupancy changes.
01:34The benefits to building owners and occupants are reduced energy costs fewer adjustments and
01:39less maintenance.
01:41Adaptive technology is offered throughout the Bryant product line and all Bryant wall switch
01:46sensors with adaptive technology feature, all digital sensing technology with a built in
01:51photo cell for daylight harvesting.
01:53Bryant offers three types of motion sensor technologies, ultrasonic us,
01:59passive infrared Pir and dual technology ultrasonic technology senses occupancy
02:06by bouncing ultrasonic sound waves off objects into space movement by a person or object
02:12causes a shift in the reflected wave frequency which is interpreted as occupancy.
02:17Ultrasonic occupancy. Sensors are good for detecting minor motion and
02:21do not require an unobstructed line of sight making them suitable for applications such as
02:26offices with cubicles or a restroom with stalls. Passive infrared technology senses occupancy by
02:33detecting the movement of body heat against the background space.
02:36It requires an unobstructed line of sight for detection and is good for detecting major
02:41motion such as walking.
02:42It works best in small and closed spaces with high levels of occupant movement.
02:47Dual technology sensors take off passive infrared and ultrasonic technologies and blend
02:53them together, maximizing reliability and minimizing the risk of false triggering.
02:57When a space is unoccupied, both ultrasonic and passive infrared technologies must detect
03:03occupancy to turn lighting on while continued detection by only one technology will keep
03:08lighting on. Dual technology is the best performing sensor
03:12in most applications and is offered throughout the Bryant product line.
03:18Lighting accounts for up to 40% of the total electrical costs in a commercial building as
03:23energy efficiency has become the key in both new and renovated commercial and residential
03:27buildings. Federal and state governments have passed
03:30regulations and created codes for increasing energy efficiency.
03:34In addition, US G BC has become a key player in the creation of the lead performance rating
03:40system for energy efficient buildings. Occupancy sensors are cited by all the codes
03:45and regulations as being a way to achieve energy savings.
03:49Bryant occupancy sensors are an excellent way to meet these requirements by reducing lighting
03:54usage from 13 to 90%.
03:57Additionally, California title 24 for residential buildings,
04:01calls for the use of vacancy sensors which must be manually turned on when entering a room and
04:06automatically turn off the lights after a person leaves the room.
04:10Bryant vacancy sensors all comply with his standard and many of the adaptive wall switch
04:15sensors are available with an external button and manual on automatic off mode enabling them
04:21to comply with California tidal 24.
04:24In order to help select the proper placement for sensors and the optimal product Bryant can
04:29provide layout assistance based upon building blueprints.
04:32Our technical service group is always available to discuss applications and troubleshoot any
04:37issues that may arise.
04:39Bryant's latest generation of sensors offers a broad range of aesthetically pleasing,
04:44technologically advanced occupancy and vacancy sensors which enable you to reduce energy costs
04:49and meet federal and state standards. Start automating savings today with Bryant
04:54occupancy and vacancy sensors. Advanced technology for maximum performance and
04:59pay back.