Transcript
00:00How to install the full coupling ID seal, cons stab fitting warning failure to
00:07follow Continentals installation instructions could result in escaping gas that could ignite
00:13and cause property damage, serious injury or death.
00:17Here are the tools and supplies you'll need for this installation.
00:35Each ID seal cons stab fitting comes shipped in a bag with printed installation instructions
00:44verify that the cons stab fitting is the correct size for the polyethylene pipe being
00:49assembled,
00:56cut the pipe ends square and make
01:03sure the pipe ends are free of dirt grease or oils in the assembly areas.
01:12Cham for both pipe ends using either Continental's ID chamfer tool with gauge or
01:18Continental's ID double ended chamfer tool.
01:22If using the ID chamfer tool with gauge check for proper chamfer by inserting pipe into the
01:28gauge up to the O ring with a proper champ for the O ring will begin to enter the pipe
01:36using the cham for tool marked the stab depth on both pipe ends
01:56stab the pipe completely into the fitting so that the mark is within 1/8 inch from the
02:02fitting entrance.
02:05Repeat for the other end to assure proper assembly
02:12and to comply with title 49 code of federal regulation.
02:15192 subpart J test requirements, the joint shall be leaked,
02:21tested. The connection is now complete.