Transcript
00:00Ok. I'm recording.
00:01It's uh number one with no tension and I think the highest we can get is 8700 here it
00:08goes for a second, right?
00:14Hey, hey, that second.
00:21Yeah. Oh, is it for one
00:27second? Have to go. Definitely.
00:34Ah but it survived.
00:41OK. Same connector.
00:42It's still hot.
00:44Uh We're gonna go now for two seconds at 8500.
00:48Here we go.
00:57Beautiful.
01:00Looks like the 2.2 seconds and looks like we fried the A CS R but
01:07the connector he is still alive.
01:11Here we go. Uh This is the pretension sample.
01:15We're gonna do one second and approximately 8500 amps.
01:20See how we do. OK.
01:32I think that was more than one second.
01:35So we just tested this one about a second and a half and the cable started to melt.
01:40Now we're just gonna hit it and see test until cable fails and then evaluate the connector.
01:46Ok. Go ahead.
02:01OK. We're gonna pause that.
02:02We'll be right back. Ok?
02:05The machines reset and now we're ready.
02:14Yes. Ok.
02:182.8 seconds.
02:20And it looks like the cable is still failed to look at the connector
02:32connector looks good. Still, here's the last set up with constant
02:38tension. We're just going to bump it to see how many
02:41amps we're pushing through that outside.
02:49What was that? 6300 right there?
02:52I'll do uh 6300 amps for a second and a half.
02:59Yeah. So I that
03:07five. Yeah, man.
03:10Well, that was that cable failed again.
03:15Look at the connectors here. Yes.
03:20And look your touches there.