Transcript
00:01The purpose of this presentation is to discuss the Fr three vegetable oil PETTS has begun
00:07incorporating as the insulating cooling medium in the transformers of some of our test
00:12equipment. I'll give a description of the fluid and
00:18explain why we're making this change. And then I'll compare conventional mineral oil
00:22to the Fr Three fluid of pointing out some of the key benefits of the Fr three and why
00:27they're important to our customers.
00:34The Fr Three Fluid is a trademark of Cargill Incorporated and is an insulating and cooling
00:39medium used mainly in distribution and power transformers.
00:43It's a biodegradable esser that's made from seed oils and other performance enhancing
00:48additives. It was formulated to minimize health and
00:51environmental risks.
00:57It's biodegradable in both soil and aquatic environments as a trademark green tint and it
01:03does not require genetically altered seed oils.
01:06It has also received an environmental technology verification from the U SEPA and is
01:12a part of the federal bop preferred program.
01:20There are several reasons why we've decided to make this change.
01:23One being an effort to work towards the Hubble sustainability initiative,
01:27which is an enterprise wide commitment to develop sustainable products and business
01:31practices. We all have a responsibility to conduct
01:35business in an environmentally friendly way with the future of conventional mineral oils.
01:40In question, this Fr Three provides an economical stable supply.
01:45While the price of mineral oil continues to rise, the price of Fr three should remain
01:49stable. And finally, as I'll discuss later, the Fr
01:53three fluid actually has multiple benefits over conventional mineral oil.
02:02So let's take a look at the traditional mineral oil that's been used in the past and obviously
02:06still being used today.
02:08It's made from petroleum and has a fire point of 100 and 55 °C.
02:13It's ignitable by electrical arcs and once ignited, the fire is self propagating.
02:18Clean up is required according to strict regulations.
02:22For example, extinguishing a vault transformer fire involves flooding the underground vault
02:27with water which then produces hundreds of thousands of gallons of contaminated water.
02:38Now let's turn to the Fr three fluid as an increased dielectric strength and because it's
02:43a 100% renewable vegetable oil accidents and spills are much less costly.
02:48There are no strict clean up regulations and this fluid is even edible.
02:53It does not contain any silicones halogens or petroleum.
02:57It actually extends the lifetime of the transformer insulating paper has increased fire
03:01and environmental safety factors.
03:08Regarding the fire safety, the Fr three has a fire point of 360 °C and
03:15even small amounts of contamination will not reduce this fire point.
03:27The fr three fluid has up to 56 times less carbon emissions and is much lower on the Ocala
03:33impact scale scoring a 7.5 versus the 1125 of mineral oil.
03:47The fr three fluid has an exceptional ability to draw out retain moisture within the
03:51transformer insulating paper and it helps prevent the paper molecules from severing when
03:57exposed to heat. Thus increasing the lifetime of the insulation
04:01paper.
04:07For example, here are the results of an accelerated life test that compares the Fr
04:12three fluid to mineral oil.
04:14Fr three fluid has been found to extend the life of the insulating paper by 5 to 8 times.
04:28Here are some other comparisons between the two fluids.
04:31Fr three has a higher viscosity as a better match of dielectric constant to craft paper
04:37insulation is a better lubricant and has a similar coefficient of expansion.
04:48We did our own test to compare the oils using the power packs.
04:51In our 880 PL DC hy pot, we measured the input voltage, input power output voltage
04:58and leakage current of a power pack containing each fluid.
05:02We found both had similar output voltages and that the power pack filled with Fr three fluid.
05:08Actually, at half the amount of leakage current
05:17we are currently using the Fr three fluid in a number of our products and will continue to
05:22expand upon this list
05:35to summarize, incorporating the FR three fluid makes for a longer lasting reliable product for
05:41our customers. And these products will help our customers meet
05:45any green initiatives that their companies may have implemented and it makes for a much safer
05:52and eco friendly product.
06:01Thank you for watching this video and please contact Hypotonic at our location nearest to
06:06you for additional information.