LAUNCHING ON 06.05.2019 AT OTC, BOOTH #3161

LAUNCHING ON 06.05.2019 AT OTC, BOOTH #3161
Breaking The Mould
For over 50 years, traditional 2ft and 4ft linear luminaires have dominated lower level lighting applications in hazardous and industrial areas. The linear shape of the enclosures was dictated by the size and shape of the fluorescent lamps they originally housed. The same shape is still in use now, but why? Retrofit some LEDs into linear enclosure and a user will be able to reap all the benefits of LED, won’t they? The truth is, they won’t.To reap all of the benefits of LED, you have to design the luminaire around them.
Discover more about LED lighting
The next generation of LED lighting
Chalmit’s largest ever investment in product development, the Protecta X is the result of:
Cutting edge design ideas
Team and skill set collaboration
Extensive research
See how LED is meant to be.
Throughout the conceptualisation, design and development of the Protecta X, these members of our brilliant team worked together to bring the next generation of LED lighting to the market. Three designers, alongside our Lighting Product Manager and Head of Product Development, worked with a dedicated Project Manager overseeing each stage. Individually, each contributed their own vast skills and expertise. Collectively, our project team are proud to bring you the Protecta X, coming in 2019.
.jpg)

.jpg)