Transcript
00:12Warning. Some reels with large or multiple springs are
00:16equipped with a ratcheted adjustment wrench follow separately instructions for its use.
00:21Failure to use ratcheted wrench on reels so equipped could result in serious personal
00:27injury warning.
00:29Do not attempt to relieve spring tension using Spanner wrench doing so may result in personal
00:35injury. Ensure that machinery to be serviced by real is
00:41at position closest to real securely mount real in desired position using three by eight inch M
00:4710 bolts.
00:49Be sure spool is aligned with cable run position, optional cable guide.
00:53If real is so equipped, see cable installation drawing,
01:00remove cover plate on spring housing to expose shaft and spring hub
01:24insert, Spanner wrench into holes in spring hub rotate wrench counterclockwise for standard
01:31rotation, number of 360 degree turns should match last digit in model number on serial
01:37plate. If model number includes nr real is reverse
01:42rotation and wrench must be rotated. Clockwise warning do not exceed number of
01:49turns indicated on cereal plate over tension can cause a broken spring sheer shaft or other
01:56damage. Remove the wrench and place back into its
02:00original shipping position.
02:24Replace access cover and gasket.