Transcript
00:05The wire con installation tool is a device to make wire terminations in self contained
00:10devices, also known as SC DS.
00:13The hazards for the wire con installation tool include the risk of electrical shock,
00:18disconnect power before installing and never wire energized electrical components do not
00:23join two different wire sizes within the same S CD.
00:26Please note only one cable at a time can be installed.
00:31The tools needed include the wire con installation tool,
00:35a screwdriver, a pair of wire cutters, a wire stripper and a receptacle back in body
00:45using the wire strippers, strip and cut the wires per the instructions,
00:52cut the sheathing and form the three wires to position it in the wire con device
01:02place the receptacle in the bottom handle cradle by aligning the bevel on the sed.
01:06And the tool bevel is a guide place the formed wires in the appropriate device terminal,
01:14squeeze the handles together to terminate the wires
01:24place the second set of formed wires into the device terminal on top of the existing
01:29terminated wires.
01:30The maximum number of wires that can exit the sed from one side is two,
01:42take the back of the receptacle and position it by aligning the bevel edge with the receptacle
01:47body. Use your hands to snap the receptacle back to
01:53the receptacle body.
01:55Listen for a double snap and do a visual check to ensure that it is latched together.
02:00Make sure the back end of the receptacle is closed.
02:03If it is too difficult to use your hand, use the handles on the wire con device by taking
02:09the back of the receptacle and placing on top of the bottom black handle position it by
02:14aligning the bevel edge with the receptacle body and squeeze the handles together.
02:30Tuck the paws in place the receptacle into the wall and align the
02:37receptacle vertically.
02:40Use the screwdriver to tighten the pulse screws
02:49place the cover plate over the receptacle.
02:54Congratulations. You have successfully installed the receptacle
02:58using the wire con installation tool.