Transcript
00:03Hawk International is proud to launch the world's first cable Gland range with an nec
00:08compliant fully transparent non metallic compound pot.
00:12This innovation represents a huge step forward for our customers as accurate installation is
00:17quickly achievable and inspection is simplified with reduced costs.
00:22Find out why the difference is clear.
00:26The main advantage that the silicon pot gives you over a metallic compound pot is you can see
00:30the resin, you can see it when you're installing it and you can see it after it's
00:34installed. So if you have any voids or any issues,
00:37they can be repaired at the time.
00:39Um You don't have to wait for the compound to set, to then inspect it and try and fix some
00:43issues with a metallic compound part. You can't see inside it,
00:46you can't see what's going on. So it's visibility of the compound number one
00:49benefit. So in terms of inspection, after installation
00:53of the resin, you can see the resin in our compound pot,
00:56you don't have to remove the pot. The resin is available for viewing in situ with
01:02the metallic compound pot, you can't see the resin.
01:04So how do you inspect it the only way to do it is to cut the pot off the resin,
01:09um to make the res in visible. But in doing that,
01:12it destroyed a sample. Traditionally, metallic compound pots,
01:15rely on maintaining flame path clearances between the gland and the pot itself.
01:20If this gap is too big, it won't prevent uh ignition with our compound pot.
01:24The silicon compound pot, it's compressible.
01:27We don't rely on maintaining a significant gap.
01:31We're compressing the component, no flame path to worry about.
01:34One of the challenges with metallic flame path is any damage to the flame path means that the
01:41product no longer complies, it's no longer safe. So therefore you either you have to discard
01:46demand any time the can compound pump, you can cut the puff,
01:51you can simply replace it.
01:53Our new range has been designed specifically for use in North America but is AEX and IE ce X
01:59certified for use globally.
02:01The range also boasts ingress protection ratings.
02:04IP 66 IP 67 IP 68 and for the first time, IP
02:1069 our nec compliant range of cable glands have been designed to provide users with ease of use
02:17whilst providing the unparalleled safety you'd expect from all Hawk International Cable glands.