Alternative Energy
Powerohm Resistors, Inc. is the leading designer and manufacturer of power resistors. We have over 100 years of engineering experience in resistor design and a proven track record of providing practical solutions for the power generation industries. Our extensive technical experiences and multiple technologies enable us to supply all types of power resistors for the renewable energy markets. For solar power, our products include photo-voltaic load resistors, harmonic filter resistors, braking modules and dynamic brake resistors. Wind power applications often use crowbar resistors, pre-insertion resistors as well as harmonic filter resistors, dynamic braking resistors and neutral grounding resistors. Our renewable energy solutions are extensively tested by a third party laboratory according to the main international standards.
SOLAR

Using the sun's energy to generate electricity is a well proven technology and resistors can help to improve these systems. During large scale installations, the solar panels are often subjected to prolonged open circuit conditions which ultimately degrade the panel’s ability to generate electricity. Powerohm has developed a portable resistive load that can be deployed temporarily during construction whereby open circuit conditions are avoided. This helps preserve a panel’s output capacity and minimizes any warranty related issues.
When the no load output voltage of a solar cell array is greater than the associated inverter that connects the panels to the power grid, it may be necessary to lower the voltage by applying a momentary load. Just as the array is to be put on line, a braking module connects a load resistor across the array until the output voltage reaches an acceptable level before enabling the inverter while simultaneously, disabling the braking module and load resistor.
Additionally, solar panels that rotate and follow the sun to ensure optimum efficiency will often use variable frequency drives to control the positioning. Powerohm braking modules and resistors will ensure that the panels stop with precision. After the solar panels produce the electricity from the sun’s rays, it must be converted from DC to AC so that it can be used by your facility and/or distributed by the utility. This requires an inverter. During this process, harmonics are produced making the electricity “dirty or contaminated”. Harmonic filters are used to clean the electricity before it goes out to the utility line and are often required by the utility. Powerohm harmonic filter resistors are a part of the harmonic filter system that achieves this.
With the addition of supplemental power sources, the need for ground fault protection has become even more important. With the use of Powerohm High Resistance Ground System, this ensures the protection your facility will need.

WIND
Modern, large scale wind turbines are very efficient at converting wind energy into electricity and often produce up to 2MW. However, with a larger scale comes more challenges from high winds and overspeed conditions. If the wind speeds become too great, the wind turbine could spin out of control. In turn, the wind turbine generates more electricity than the grid or batteries can handle. The grid is a finite element, with a finite capacity. However, it has to accommodate a wide swing of current draws. For wind turbines charging batteries, the same effect occurs. Batteries have a finite capacity, yet they have to accommodate wide swings in current draws. Stabilizing the power output of windmills to match the current draw is done using load resistors. A load resistor dissipates the excess electricity. Usually, a charge controller or voltage regulator is used to determine how much power is diverted to the load resistor. For a battery charging system, the load resistor is used to prevent overcharging the batteries.
Wind energy use brings problems of voltage fluctuation and harmonic distortion. One of the sources to these distortions is the AC-DC-AC full size converters. Harmonic filters reduce the total harmonic distortion (THD) and enhance the power quality. Powerohm harmonic filter resistors are a part of the harmonic filter system that achieves this.
Wind Turbines must be facing into the wind for optimum wind energy generation. Small turbines are pointed by a simple wind vane, while large turbines generally use a wind sensor coupled with a servo motor. The use of electric drives for their positioning system is often used. The drives use Powerohm braking resistors to ensure that the turbines stop where required.
With the addition of supplemental power sources, the need for ground fault protection has become even more important. With the use of Powerohm High Resistance Ground System, this ensures the protection that your facility will need.