Transcript
00:08This is a professionally installed electrical box.
00:12The electrician took pride in his work keeping the interior of the box free from debris and
00:18wires neatly arranged in the box prior to device insulation,
00:22then the mud hits the box wires are cut.
00:27The opening in the box was left unprotected by the electrician.
00:31And what was a clean meat installation becomes a clean up,
00:36fix up problem for the sheet rocker. Successfully finding the outer boundaries of
00:41the unprotected mud ring can be costly.
00:44The bit goes inside the mud ring dulling or breaking the router bit as it seeks the outer
00:49edges looking for the mud ring outline is time consuming expensive and probably
00:56results in damaged sheet rock that will need to be replaced.
01:00The electrician or sheet rocker has resorted to various primitive time consuming and hazardous
01:06methods to protect the interior of the box from using cardboard to stuffing sheets of the local
01:12paper inside these and other methods have never proved satisfactory and all are costly.
01:19So the struggle has continued since the days of Edison.
01:24The solution.
01:25The reo protect cover for single and two device mud rings,
01:30simple, quick to install and reusable by either an electrician or a sheet rocker.
01:36The hardy steel cover protects the interior of the box from damage and debris.
01:42The variety of protect covers which seal the entire mud ring opening will protect work.
01:47Even when devices such as outlets. GFS, decora switches and toggle switches are
01:53already installed.
01:56Protect covers for low voltage installations and removal are so easy and quick.
02:01Even a novice can do it and the cover allows the low voltage wiring to be tied off on the
02:07rear of the cover so that wiring does not get lost in the wall cavity.
02:13Electricians and sheet rockers protect your work.
02:17Electricians protect your wires from the minor wire.
02:20N which can result in a huge expense. Protect the interior of the box and keep it
02:26clean of debris.
02:27Sheet rockers cut the time looking for the perimeter of a mud ring.
02:31Protect yourself from excessive sheet rock damage, protect router bits from dulling or
02:37breaking the rao protect cover, eliminates this, this,
02:45this this and this use
02:51the rao protect cover and both the electrician and the sheet rocker can have a good day.
03:02Protect covers a product where everyone benefits.