Solutions OverviewComprehensive solutions for commercial, residential and industrial applications.
Markets OverviewRACO® serves the needs of customers in a variety of market applications. See our major markets and building types below.
Transcript
00:11Innovating and producing quality electrical boxes and covers for over 100 years also offers
00:16a full line of crushed corner covers for four inch square boxes,
00:20ideal for exposed work environments including situations with surface mounted boxes.
00:26The covers enclose the electrical box, securing wiring connections.
00:29While also providing a means to mount a variety of electrical devices.
00:34Choose from 19 covers preconfigured for specific two gang device combinations,
00:39any single gang device or blank cover or for added flexibility.
00:43Select one of the three universal covers that include adapter plates for more options during
00:48installation, rao crushed corner covers are drawn from heavy duty galvanized 16 gauge steel
00:54and include any required screws when applicable.
00:59Let's run through a typical installation. So you can see some of the handy features
01:03before starting any electrical work first, make sure the power is off at the load center or
01:08breaker panel, prepare the device for mounting by removing the ears from the mounting strap or
01:13yoke by bending back and forth a few times at the perforation.
01:17For most receptacles also remove the ends of the strap at the perforation.
01:22If you don't see the perforation, it might be necessary to snip the pieces off with a cutting
01:26tool, avoid removing too much strap to maintain the integrity of the device,
01:31mounting holes.
01:32Now wire the device or devices per manufacturer instructions, secure the device to the cover
01:38using the device mounting screws that come with the cover or device,
01:42the threaded tabs wedge against the edge of the cover allowing for a tight connection without
01:47holding a nut, remove the two cover mounting screws that came with the four inch square box
01:52roll or tuck the conductors into the electrical box.
01:55So the cover can be screwed down for universal covers.
02:00Select the appropriate adapter for your needs.
02:03Remove the device, mounting screws that comes with the device,
02:07add the adapter to the face of the device and sandwich it to the cover with the mounting
02:11screws. Repeat for other devices if applicable,
02:15that's it. The crushed corner cover is now ready to
02:18deliver a lifetime of rugged protection.
02:20Always look to Hubble rao for all your electrical needs.