Transcript
00:07Rao. The market leader in electrical boxes has added
00:10the stabbed two series of 4, 1116 square boxes. This expands our existing line of stabbed boxes
00:16which is already preferred by professionals for its built in connectors which offer a three
00:20times faster install for flexible armored cable. Of course,
00:23the larger four and 11/16 opening provides more capacity than the four inch models for
00:28situations with bigger cables, multiple conductors, larger devices or whenever the
00:33larger opening is just preferred just like the original stait.
00:37The stait two includes our unique built in connectors, but we've added a few more
00:41enhancements for more options and time and labor savings.
00:45First off each stait connector handles three cables instead of two and the connector accepts
00:50larger cables than before plus stait two connectors now include individual release
00:55screws, providing added convenience if any one cable needs to be removed.
01:00And the boxes include our TKO an eccentric knockout for either half inch or three quarter
01:05inch on the same side as the cable connector.
01:08Another helpful feature are the bracket options like the M bracket,
01:12which is designed with a 38 inch deep offset allowing for quick and easy face mounting from
01:17either side, which is especially useful between narrow stud openings or the CM or cable
01:22management bracket, which provides a quick means of securing the cable at the box entry
01:27for the National Electric code.
01:29Today, we'll walk through a typical install of the 252 MS CM and I'll show you a few of the
01:34stait two features in action as well as demonstrate the time saving benefit of the
01:38entire stait line.
01:40We're here in a new work environment. Although there are some one gang stait switch
01:43boxes designed specifically for old work. If your job is a remodel or similar situation
01:48as with any electrical work, make sure the power is off at the breaker for this install.
01:54We're using 14 3 and 10 3 MC cable start by fastening the bracket to the metal stud and
01:59then removing the necessary pry outs with the cable already stripped,
02:03run the loose wires into the box through the open pry out,
02:06pushing until you feel it lock in place.
02:09I'll do the same for the other cables in the event that something changes and you need to
02:13remove a cable, simply loosen the connector screw and the cable will release the 252 MS CM
02:20includes the handy cable management clip. So I'll attach the cable which provides the
02:24first means of support for the MC cable and that's all there is to it efficiently installed
02:29in under a minute. Compared to 2 to 3 minutes using traditional
02:32methods. In addition to this 252 MS CM box, the stait
02:36two series includes these five other four and 1116 boxes,
02:40all part of the Reo Stait line, which now includes 23 box options to reduce the time and
02:46labor on almost any job.
02:48So if you want to save time and reduce clutter on your next project,
02:52ask for Reo's stab it and stab it two boxes.
02:55And remember for any of your commercial, industrial or residential projects,
03:00look to Hubble Rao for proven and trusted solutions.