Transcript
00:00Bernie understands that proper connector installation is a vital part of a connection's
00:05longevity efficiency and safety to help provide all the necessary information to make a
00:10connection using the Burnie engineered system.
00:13Burnie developed Bendy Connect. This app provides installers with tooling dye
00:18and connector installation information to make a connection.
00:21Right. The first time installers will first open the
00:24Bernie connect app in the module options, click installer info.
00:29When making a connection to use the installer info module.
00:33Users simply supply four pieces of information and the app will do the rest.
00:38In this example, the installer is presented with the following connector material is copper
00:44connector type code class B or C conductor size four A awg
00:54connector material, copper. The installer will select the installation
00:58criteria in the app. The results will display only applicable
01:02installation tooling series and provide the installation details based on the tool selected
01:08users can swipe to the right on the installation tools to see more tooling options
01:13from the tooling menu. The user can select a different tool and the
01:17installation details will dynamically update with the appropriate information.
01:21The installation details will display installation tool series selected connector
01:27tube designation, color code, dye index number, if applicable dye catalog number,
01:33if applicable crimp dimensions, if applicable. And an illustration of a standard and long
01:39barrel termination with proper number of crimps, proper crimp location and proper direction.
01:45If the user swipes up there is an expanded ranges section that shows our dial as tool
01:50options. If applicable for additional support,
01:53the play button in the upper right hand portion of the installer info module will display
01:58installation videos for the installer.
02:01Bernie connect, bringing the Bernie engineered system to the palm of your hand,
02:06giving you real answers in real time while helping you to simplify the connection and
02:12inspection process. Download Bernie Connect today from your devices
02:15app store. Thank you for watching this Bernie connect
02:18inspector module.