Take a TourHere is a glimpse of Burndy’s Solutions for the different Markets.
Take a TourA quick look through the various markets we are equipped to cater to: browse Burndy Markets
Transcript
00:13Today, we'll be using A Y GB on a four rock conductor to 1/4 inch bus bar.
00:19First measure the conductor.
00:27Next select a Y GB bus bar connector based upon the size of the conductor and the thickness of
00:34the bus bar you were working with.
00:35Today, we'll be using a YG 14 BT C 28 position the connector onto the bus bar,
00:43insert the conductor into the connector
00:55place the connector into the center of crimping dyes that are placed in the tool head,
01:00crimp the connection until you hear an audible click from the pat 750 indicating the tool has
01:06gone full cycle and the crimp is complete,
01:13visually inspect the emboss against the connector markings to validate a proper
01:18connection has been made. Your Y GB connector is installed for more
01:23information. Visit burnie.com.
01:26Thank you.