Take a TourHere is a glimpse of Burndy’s Solutions for the different Markets.
Take a TourA quick look through the various markets we are equipped to cater to: browse Burndy Markets
Transcript
00:13Today, we'll be installing a YGHP on a 40 conductor to number three rebar,
00:20first measure the conductor.
00:23Next measure the rebar and determine the appropriate connector based on the conductor
00:29and rebar size you are working with. In this example,
00:32we are using a YGHP 29 C 29 insert the
00:39conductor into the tap side of the connector,
00:50then place the rebar into the run side of the connector,
00:56align the connector into the center of the crumping dyes that are placed in the pat 750
01:01tool head crimp the connection until you hear an audible click from the pat 750
01:08indicating the tool has gone full cycle. And the crimp is complete,
01:24visually inspect the dye emboss on the connector to validate a proper connection has
01:28been made. Your YGHP connector is installed for more
01:33information. Visit burnie.com.
01:36Thank you.