Take a TourHere is a glimpse of Burndy’s Solutions for the different Markets.
Take a TourA quick look through the various markets we are equipped to cater to: browse Burndy Markets
Transcript
00:15The following is an instructional video on how to install the YSHG family of connectors.
00:21Today, we'll be using a YSHG 3434. Note, these connectors can be
00:27installed using the PAT 750 Y 750 Y 45 or Y 46 and
00:34pat 46 with recommended dyes.
00:37Other Bernie tooling options may be available contact Bernie for more information,
00:43determine the rebar size, determine the conductor size,
00:51choose appropriate connector of required size based on conductor size,
00:56rod size or rebar size position, the connector on rebar and conductor
01:07place the Burnie U 1104 crimping dye in the pat 750 L I
01:15begin crumping the connector on the inside edge of the connectors slot.
01:23Now crimp the other inside edge of the connector slot,
01:30place a 3rd and 4th cramp on the outside edges of the connector,
01:43inspect the emboss and compare to dye marking on the connector to confirm a proper connection
01:49was made for more information about the Burnie high ground YSHG
01:553434 and other Bernie products visit bernie.com