Jefferson County Historical High School
Project
Rehabilitation of the historic school built in 1852 located in Monticello, FL.

Background
Built in 1852, the Monticello High School (also known as the Jefferson Academy and Jefferson County High School) was the first brick public school built in Florida. The school was built under the direction of Samuel Carroll, a builder/plantation owner from Virginia using locally made bricks fired in a kiln at the George Taylor Plantation. The school was added to the National Registry of Historic Places in 1999 but has been vacant since 1991 due to needed repairs. The State Legislature approved funding for the historic school rehabilitation in 2010.
Problem
The plans called for shoring of the existing floor system and roof trusses to use the lower level as a museum and the second story converted into courtrooms. Soil testing identified layers of highly plastic clays, therefore requiring a deep foundation solution to support the design.

Solution
CHANCE® helical piles were the best deep foundation solution for this application because they can be installed easily in areas with limited access utilizing hand-held or small construction equipment. CHANCE type SS150/RS2875.276 helical combo piles with a single 6″ helix were specified to support the new footings and girders. The combo pile consists of a square shaft lead section and a round shaft extension. The square shaft is better suited to penetrate dense soil. The round shaft extensions offer more lateral resistance with more of the shaft exposed to the surrounding soil. The hollow round shaft extensions can also be filled with grout to increase stiffness and to help protect against corrosion.
Deep Pile Foundation - Custom Mobile Unit Installing Pile
The piles were installed with an Eskridge 8K drive-head that was mounted on a Boxer 320 Compact Utility Loader and for the less accessible areas a custom built mobile unit was used. New construction caps were added to the piles for connection to the poured concrete footings and a specially designed walkway style bracket was added to the piles to allow for connection to the new wood support beams.
Pile depths ranged from 20-22 feet below existing grade with 18KIP working load in compression. Final installation torques were 4,800 – 5,200 ft-lbs. Helical pile installation took approximately three weeks to complete.
Key Benefits:
- LIMTED ACCESS
- TIME TO INSTALL FASTER THAN CONCRETE
- STANDARD EQUIPMENT FOR INSTALLATION
- LABOR SAVINGS – SMALLER CREWS
- NO SPOILS TO REMOVE
- INCLEMENT WEATHER INSTALLATION
- IMMEDIATE PROOF TESTING AND LOADING
- LOW TO NO VIBRATION/NOISE