Take a TourBenefits are derived from well implemented Solutions. The challenge to save energy, improve safety or make sure everything continues to perform in a harsh environment, are all candidates for good solutions.
Take a Tour of the Markets We ServeHubbell serves the needs of customers in a variety of market applications. See our major markets and building types below.
Transcript
00:06The dashboard provides you the most important controls for socket tapping on socket will
00:11bring you to its details screen where you can access full control of socket.
00:15Socket's detail screen offers controls for the le night light.
00:19You can see the current le color and quickly turn it on and off tapping on the night light
00:24will bring you to the precision controls for it. On the socket nightlight detail screen,
00:29you get a great preview of your socket led. The color slider bar allows you to quickly
00:34scroll through the virtually infinite color options, brightness and saturation,
00:38give you the ability to tweak the color to perfection.
00:41Quick colors were designed to give you easy access to some of the most popular moods and
00:45tones. In addition to the bright colors, the default
00:49options give you a selection of colors balanced to match other typical light sources or
00:53simulate natural light.
00:55You can even save your favorite color settings to keep them handy or to add that color to
01:00multiple sockets, simply tap add in quick colors.
01:04The current setting will be carried over and you can adjust if needed.
01:08Give your quick color a name and then tap. Save your quick color will be added to the list.
01:14You can also manage your quick colors by tapping, edit on quick colors.
01:18This will bring up a list of the quick colors and you can tap into the color you want to edit
01:23or remove sockets. Led nightlight can be added to scenes and
01:28schedules as well. So you can have your custom lighting happen
01:31automatically if you want to learn more about I devices, socket or need additional help.
01:36Make sure to head over to I devices. Inc.com/support.