Transcript
00:00I devices, wall outlet has been designed to make it simple and quick to get set up in a few
00:07short steps. You'll transform your wall outlet into a
00:10connected wall outlet in the box. You will find the I devices wall outlet
00:15installation guide as well as a few wire nuts. To help with your installation to install,
00:20you will need a flathead screwdriver, a Phillips screwdriver,
00:23a voltage detector and pliers.
00:26The I devices wall outlet fits any standard size rock or face plate so you can select one
00:32that works best for your home.
00:34If the wires in your gang box differ from the installation described in this video or you are
00:39unclear at any point of the installation process, please consult a qualified licensed
00:44electrician I devices while outlet must be installed in a manner that conforms to all
00:49applicable national state and local building codes turn off the power to the circuit at your
00:55breaker or fuse panel.
00:57If you are replacing an existing outlet, verify that the outlet no longer has power before
01:02proceeding, using a voltage detector.
01:06Now unscrew and remove the face plate from the existing outlet.
01:16Next, remove the two screws that secure the outlet to the gang box.
01:32Carefully pull on the outlet to remove it from the gang box.
01:38Take a photo of your existing wiring for future reference,
01:45disconnect your old wall outlet by unscrewing and removing the existing wires
01:57wherever possible. Install the I devices wall outlet in a non
02:01metallic gang box and use a non metallic face plate as metal gang boxes and face plates can
02:06decrease the wi fi signal strength.
02:16When installing the I devices, wall outlet, connect the black wire on the back of the wall
02:20outlet to the line wires which are typically black with the provided wire nuts.
02:25If there are multiple black wires cap them all together.
02:29Next, connect the white wire on the I devices, wall outlet to the neutral wires which are
02:34usually white with the provided wire nuts. If there are multiple white wires cap them all
02:39together, lastly connect the bare copper ground wire on the I devices,
02:44wall outlet to the ground wire which is usually copper or green in color.
02:49Ensure all wire nets are securely fastened carefully, push the wires into the gang box and
02:55install the wall outlet into the gang box. Taking care not to pinch any wires,
03:03secure the I devices, wall outlet into the gang box with the provided screws.
03:12It's best to start both screws before tightening to keep installation easy and ensure
03:17the outlet is straight.
03:28You can now install your selected face plate, the I devices,
03:31wall outlet fits any standard size rocker face plate, so you can select one that works best
03:37for your home. Turn the power back on at
03:44the breaker. If the outlet is connected properly,
03:47you should see the led indicator rapidly flash blue to indicate the unit is ready to connect
03:52to the app, launch the I devices connected app and you will be guided through the process of
03:57connecting your I devices product for IOS devices.
04:01You will need the home kit, set up code on the pull out tab on your product.
04:11Congratulations. Your wall outlet is installed.
04:14You're now ready to connect to your wireless network.
04:19If you want to learn more about I devices outlet or need additional help.
04:23Head over to I devices. Inc.com/support.