Take a TourBenefits are derived from well implemented Solutions. The challenge to save energy, improve safety or make sure everything continues to perform in a harsh environment, are all candidates for good solutions.
Take a Tour of the Markets We ServeHubbell serves the needs of customers in a variety of market applications. See our major markets and building types below.
Transcript
00:06For I OS users. If you have multiple locations where you use
00:10your I devices products such as a primary residence and also a vacation home or office,
00:16you can create multiple homes in the I devices connected app to stay organized.
00:21If you choose to share home control with other users, you will need to invite them to each
00:26home. You wish for them to have access to to get
00:30started on the home dashboard. Tap the current home name in the upper left
00:35hand corner, next tap, switch home in the upper right hand corner,
00:40tap, create new name, your new home or choose a name from the suggested name
00:46list, customize a photo or choose the default photo.
00:52Confirm the location of the new home or enter an address,
00:56then tap add tap done and your new home is now set up.
01:03When you're using the latest version of the app, your home will switch automatically for you
01:08based on your location.
01:10You can also switch homes anytime by tapping on the home name in the upper left corner of the
01:15dashboard, then tapping on switch home.
01:21If you want to learn more about I devices products or need additional help head over to I
01:26DEVICES. Inc.com/support.