Take a TourBenefits are derived from well implemented Solutions. The challenge to save energy, improve safety or make sure everything continues to perform in a harsh environment, are all candidates for good solutions.
Take a Tour of the Markets We ServeHubbell serves the needs of customers in a variety of market applications. See our major markets and building types below.
Transcript
00:01Congratulations on your purchase of your new Hubbell Basket Tray Wire Management System.
00:14Today, we will be comparing the new Hubbell preformed 90 degree fitting with a more
00:19conventional 90 degree field sweep.
00:21You will need a 7/16 inch hex nut driver, six HBTSK splice kits,
00:28a marker, Hubbell HBT cut tool basket tray cutter, HBTR
00:330412 90 degree tray, Hubbell HBT0412 wire basket tray
00:42to make a conventional 90 degree sweep.
00:45First identify with a marker which segments of the tray to cut,
00:49remove six for a 4 by 12 tray cut. The tray is
00:56marked, repeat for the opposite side
01:04carefully bend the tray to create the 90 degree sweep.
01:07Closing the gaps of the inside radius, fasten the splice kits to the sides of the inner
01:12radius. Ensure the threads face outward
01:24steps to assemble a Hubbell 90 degree preformed fitting face,
01:29the part that dips down into the wire basket tray and secure it down into place so that they
01:34intertwined place your carriage bolt in the hole located on top of the base.
01:56Repeat for the opposite side
02:10lock, the provided long outside wall into tray sides and lock it into the precut slots in the
02:15base.
02:26Repeat for the short wall finish securing fitting walls by bending tabs
02:33under fitting base
02:54using a Hubbell, preformed 90 degree fitting speeds up the installation by 3.5 times.
03:01Preformed fittings provide labor and time savings, more consistent installations and can
03:06be installed directly in the wire basket run.
03:10Thank you for viewing our installation video for additional information,
03:14contact your local Hubbell Wiring Device.
03:17Kellems rep.