Take a TourBenefits are derived from well implemented Solutions. The challenge to save energy, improve safety or make sure everything continues to perform in a harsh environment, are all candidates for good solutions.
Take a Tour of the Markets We ServeHubbell serves the needs of customers in a variety of market applications. See our major markets and building types below.
Transcript
00:05Kellems has several series of grips for use with fiber optic communications cable.
00:10These grips include pulling grips with built in swivels, grips with steel ends to protect
00:15fragile cable ends, grips with low profiles to pull cables in tight places.
00:21And the OPTISOK an effective tool to place pre terminated cables also available are grips
00:27to support fiber optic cable.
00:30Wire rope grips are used for changing wire rope on oil derricks,
00:34large cranes, overhead cranes and drag lines.
00:38It provides a quick safe, inexpensive temporary splice by installing the used wire rope in one
00:45end and the new rope in the other. The new wire rope can be pulled in as the old
00:50one is pulled out.
00:51Splicing grips are used as a temporary splice for rope cable or wire rope.
00:57They can also be used as cable reinforcement and can act as a shield to protect cables and
01:02hoses from abrasion. Conduit riser grips are permanently fastened to a support ring
01:08resulting in a one piece unit which will allow air ventilation within the conduit.
01:13The entire grip is supported by the conduit itself and no other hardware is required.
01:20Kellems hose containment grips are designed to stop this industrial hazard before it starts-
01:25suppressing the violent whipping action of a snapped high pressure hose,
01:29holding it steadfastly in place and allowing it to expend its dangerous kinetic energy in a
01:36controlled and safe manner.
01:38Kellems grips can be customized to accommodate any application.