Take a TourBenefits are derived from well implemented Solutions. The challenge to save energy, improve safety or make sure everything continues to perform in a harsh environment, are all candidates for good solutions.
Take a Tour of the Markets We ServeHubbell serves the needs of customers in a variety of market applications. See our major markets and building types below.
Transcript
00:03Introducing Hubbell's new Concrete Extend Caps for recessed concrete floor boxes,
00:08for applications like stained or polished concrete and for pores with larger aggregate
00:13Hubbell's new one half inch extend caps can be stacked to create up to one inch concrete above
00:18the box which will also help to prevent surface cracking under heavier loads.
00:23Accommodating our 2, 4, 6 and 10 gang series boxes. Each box ships with one extend
00:29cap and a second extend cap can be purchased separately.
00:32The extend caps are easy to install during pre pour phase of the installation featuring four
00:38pockets on the top side of the cap as well as four integral pins on the underside of the cap.
00:43The unit is simply locked together for easy installation.
00:47The pocket in the concrete that the caps create becomes an extended access space upon which the
00:52flanged surface covers will fit into. The flush covers, nest into the pocket even to the
00:57finished floor with the aid of weight bearing backing nuts supplied with the cover,
01:01mounting screws. For more information visit hubbell.com.