Transcript
00:01Introducing Hubbell's newly redesigned line of H Moss occupancy and vacancy sensors.
00:07Utilizing tomorrow's technology today.
00:10H Moss is a complete line of occupancy and vacancy sensors including wall switches,
00:16wall mounted sensors and ceiling sensors designed for a broad range of applications in
00:22both commercial and residential settings, such as offices,
00:26hallways, lobbies, classrooms, large gathering areas, restrooms,
00:32small closets and pantries. Anywhere. There's opportunity for energy savings
00:40Moss features the latest technological advances including its breakthrough adaptive technology
00:46and its dual technology, motion sensors that use both passive infrared and ultrasonic
00:52technologies together for maximum coverage and flexibility.
00:57These sensors are a perfect solution for reduced energy costs,
01:01fewer adjustments and less maintenance.
01:05Adaptive technology is a Hubbell breakthrough that delivers a true install and forget
01:10operation. Adaptive technology sensors use microprocessor
01:15technology that constantly monitors the area and automatically adjust the sensitivity and
01:21timer based on activity.
01:23It literally fingerprints, movements, motion patterns and occupancy habits by recording them
01:30in memory. By choosing adaptive technology sensors,
01:34you no longer have to make manual adjustments for furniture layout,
01:37seasonal changes or occupancy changes.
01:41The benefits to building owners and occupants are reduced energy costs,
01:45fewer adjustments and less maintenance.
01:50Adaptive technology is offered throughout the H MOSS product line and all H mos wall switch
01:55sensors with adaptive technology feature. All digital sensing technology with a built in
02:01photo cell for daylight harvesting Hubbell offers three types of motion sensor
02:07technologies, ultrasonic, passive infrared and dual technology.
02:14Ultrasonic technology senses occupancy by bouncing ultrasonic sound waves off objects in
02:20a space movement by a person or object causes a shift in the wave frequency which is
02:26interpreted as occupancy.
02:29Ultrasonic occupancy. Sensors are good for detecting minor motion and
02:33do not require an unobstructed line of sight making them suitable for applications such as
02:38offices with cubicles or a restroom with stalls.
02:43Passive infrared technology senses occupancy by detecting the difference between body heat and
02:49the background space.
02:51It requires an unobstructed line of sight for detection and is good for detecting major
02:56motion such as walking.
02:58It works best in small enclosed spaces with high levels of occupant movement.
03:04Dual technology sensors take both passive infrared and ultrasonic technologies and blend
03:10them together, maximizing reliability and minimizing the risk of false triggering.
03:15When a space is unoccupied, both ultrasonic and passive infrared technologies must detect
03:22occupancy to turn lighting on while continued detection by only one technology will keep
03:28lighting on. Dual technology is the best performing sensor
03:32in most applications and is offered throughout the H Moss product line.
03:37Lighting accounts for up to 40% of the total electrical costs in a commercial building.
03:42As energy efficiency has become the watchword in both new and renovated commercial and
03:47residential buildings. Federal and state governments have passed
03:50regulations and created codes for increasing energy efficiency.
03:55In addition, lead has become a key player in the creation of design standards for energy
04:01efficient buildings.
04:03Occupancy sensors are cited by all the codes and regulations as being a way to achieve
04:09energy savings.
04:10H Moss occupancy sensors are an excellent way to meet these requirements by reducing lighting
04:16usage from 13 to 90%.
04:20Additionally, California title 24 for residential buildings,
04:25calls for use of vacancy sensors which must be manually turned on when entering a room and
04:30automatically turn off the lights after a person leaves the room Hubble vacancy sensors
04:36all comply with this standard. And many of the adaptive wall switch sensors
04:40are available with an external button and manual on automatic off mode enabling them to
04:47comply with California T 24.
04:50In order to help select the proper placement for sensors and the optimal product Hubble can
04:55provide layout assistance based upon building blueprints.
05:00Our technical service group is always available to discuss applications and troubleshoot any
05:05issues that may arise.
05:07Hubbell's latest generation of Hubbell H Moss sensors offers a broad range of aesthetically
05:13pleasing, technologically advanced occupancy and vacancy sensors which enable you to reduce
05:19energy costs and meet federal and state standards.
05:23When you choose Hubbell H Moss occupancy sensors, you're using tomorrow's technology today.