Transcript
00:10This video will show how to select the correct anchor tools to fit your truck and install the
00:16tough one in Pisa style anchor.
00:18There are four anchor tool components used to drive the tough one in Pisa anchors.
00:23The first component is the Kelly Bar adapter.
00:26It is used to attach the anchor drive tools to the truck's Kelly Bar.
00:29Chance. Kelly Bar adapters are supplied with a bent arm
00:32pin and coil lock.
00:34Additional pins and coil locks can be purchased separately.
00:38The second component is the torque indicator, choose either the digital torque indicator
00:43shown here or the sheer pin torque limiter.
00:47The third component is the locking dog assembly. It is used to attach the anchor driver wrench
00:53and hold the anchor in place during installation.
00:56The fourth component is the anchor driver wrench that attaches to the anchor.
01:00There are two sizes of anchor installation tools based on their torque capacity,
01:05pick the size based on torque capacity of truck and anchor size.
01:09If your truck's torque motor has a torque capacity over 10,000 ft pounds,
01:14you should look to use the tough one line of anchor tools rated at 15,000 ft pounds.
01:20Some anchors such as the 15,000 ft pound rated tough one anchor require the 15,000 ft pound
01:27tooling. It is important to note that the 10,000 ft
01:30pound tooling has a five and a quarter bolt circle and the 15,000 ft pound tooling has a
01:36seven and 5/8 bolt circle. An anchor tool selection guide can be found at
01:40Hubble Powers systems.com and can help you pick the correct tooling required based on the
01:45anchor you plan to install. First, let's determine the proper Kelly Bar
01:49adapter for your truck measure the distance across flats.
01:53This Kelly Bar measures three inches across the flats, measure the distance from the center of
01:58the hole to the end of the Kelly Bar.
02:00The distance from the flange of the Kelly Bar adapter to the center of its hole needs to be
02:05the same or longer to allow the flange of the Kelly Bar adapter to fit below the end of the
02:10Kelly Bar. Use the product information found on Hubble
02:13Power systems.com to pick the correct Kelly Bar adapter.
02:17The next component is the torque indicator.
02:19A torque indicator is used to measure torque and determine anchor holding capacity,
02:24pick the corresponding 10,000 ft pound or 15,000 ft pound walking dog assembly.
02:29There is only one catalog number for each torque rating.
02:32The C 3030069 HD is used with 10,000 ft pound tooling
02:39and the C 3030981 is used with a 15,000 ft pound tooling.
02:46Next pick the anchor drive wrench, starting with the 10,000 ft pound rated tools.
02:51There are two wrench sizes. The C 1021583 has an orange band painted on the
02:58end. It fits the tough one anchors with a two and a
03:01quarter sock and the Pisa anchors with the one and 38 square hub.
03:06The C 3031064 has a yellow band painted on the end.
03:11It fits the tough one anchors with a 2.5 inch socket and the Pisa anchors with a 1.5 inch
03:16square hub for the 15,000 ft pound rated tools. There is only one wrench size.
03:23The C 3030983 has a red painted band on the end. It fits the tough
03:30one anchors with a 2.5 inch socket and the Pisa anchors with a 1.5 inch square hub.
03:36Anchor drive wrenches are available in 3.5 ft and 7 ft lengths for all styles of drive
03:42wrenches see Hubble power systems.com. For more details,
03:46an extension wrench can be used to install anchors to depths greater than 7 ft.
03:51The extension wrench is attached to the top of the drive wrench to summarize the anchor tool
03:55selection process. First determine if 10,000 ft pounds or 15,000
03:59ft pound tooling is required, determine the correct size.
04:03Kelly Bar adapter, choose your locking dog assembly and choose the correct drive wrench
04:09and extension assembly.