Transcript
00:03Using Hubble power systems. Verso programmer,
00:06the versa. Reclosing is as simple to program as it is to
00:10install with a windows based computer or an ipad.
00:13The VERSO can be programmed prior to installation or after installation at any time.
00:19An instruction manual included with each rec closure provides step by step instructions on
00:24how to connect to and program the various settings specific to each type of versa.
00:29Reclosing once a connection is established with a Verso rec closure,
00:33a main screen with basic rec closure settings is displayed under a settings tab for example,
00:39familiar reclosing parameters of minimum trip reset time TCC curves,
00:45number of trips before lockout sequence, coordinations and other parameters are shown
00:50starting on the left side of the settings. Tab, the verso rec closes or minimum trip value
00:56is the over current value at which the reclosing will trip.
01:00The minimum response time is a predetermined time that the rec closure must wait to trip.
01:05If this time exceeds the value of the TCC curve, then the rec closure will trip at the minimum
01:10response time. However, if the TCC time exceeds the minimum
01:14response time, it will be ignored and the rec closure will trip on the TCC curve.
01:19This can be used, for example in co ordination. When there is crossover in the TCC curves at
01:25higher trip values, the reset time is the time before the incremented shot or trip count is
01:31zeroed out and a new set of reclosing cycles begins.
01:35The handle delay feature is unique to the versa, reclosing and provides journeymen with added
01:40safety when closing a circuit such as time necessary for the journeyman to clear the area
01:45and safely remove the hook stick by toggling the yellow handle back to the up position.
01:51The user initiates closing the circuit but the handle delay introduces a delay to closing the
01:56internal contacts of the vacuum bottle for the programmed amount of time.
02:01Next. The cold load time is the amount of time that
02:04the rec closure will not trip up to the cold load pickup value when the contacts are closed
02:09from a lockout state, ie when the yellow handle is used to manually close the contacts.
02:14If an over current is detected during the cold load time and above the cold load pickup value
02:20then reclosed will trip on the program TCC two curve.
02:24The cold load pickup value is a multiplier of the minimum trip.
02:27For example, if the cold load pickup is programmed to two and the minimum trip is
02:32programmed to 100 amps, then the reclosing must see at least 200 amps in order to trip during
02:38the cold load time on the TCC two curve below. These settings are the rec close operation trip
02:44or shot. Specific settings of enabling the minimum
02:47response time which TCC curve TCC one or TCC two to use the rec close interval,
02:53open time between shots whether sequence coordinations should be enabled.
02:57And the overall number of program shots before a lockout enabling sequence co-ordination
03:03allows for the rec closure to increment its count on that shot even though the program TCC
03:08time is not met. And the rec closure does not rec close or
03:12operate. This can be used when the rec closure needs to
03:15keep in sequence with a downstream rec closure that is operating in order to prevent
03:19additional blinks if that downstream rec closure fails.
03:22If sequence coordinations lockout is enabled, then the rec closure will lock out on the fifth
03:28over current event.
03:29Perhaps the most unique feature of the VERS rec closure is the ability for the user to program
03:35the one shot or non rec closure red handle functions on the device.
03:39The NR handle may be programmed in either one mode or two modes.
03:43If the rec closure is programmed to one single mode, then every time that the NR handle is
03:48toggled down, the rec closure will be in that one mode.
03:51If the verse is programmed to two or dual mode to put the rec closure in the first program
03:56mode, simply toggle the red handle down to put the rec closure in the second mode,
04:01toggle the NR handle down up down within 30 seconds.
04:05The versa can have one NR mode and one HLT mode program through the U I.
04:11Whenever the HLT mode is selected, the beacon will flash indicating to the user that the unit
04:16is in HLT and not in our mode.
04:19If the verse is in a one shot mode, the reclosing state will indicate that mode in the
04:24U I. Finally, the user may choose up to two TCC
04:29curves to program on up to four shots or rec close operations,
04:34all versa. Reclosing offer a standard set of 11 curves
04:37each having three modifiers which are stored on the rec closure control dependent on the versa
04:43type and version. There can also be either four or 10 additional
04:47curves stored on the control board.
04:49Additionally, the versa XC and two reclosing include a TCC editor within the U I in which
04:56manual or custom curves can be added to the rec closure control and or stored in the U I for
05:01later programming.
05:03If operating a versa two or verso XC reclosing.
05:07Additional advanced settings are also available in the U I under the set up,
05:11drop down menu located at the top left of the window.
05:14The user can choose to modify when the reset time begins,
05:18enable symmetric and or asymmetric in rush enable or disable low battery mode and access
05:24the skat a modem utility for modifying modem settings.
05:27Additional details about these settings can be found in the versa XC instruction manual.
05:34The next tab selectable in the U I is the real time monitoring tab which displays various root
05:39mean square or R MS current values measured by the rec closure if connected to the reclosing
05:45wirelessly and when installed on a loaded line, the now value provides the R MS current scene
05:51in amper up to the maximum nominal load for the reclosed type.
05:55The verso 12 and Xe reclosing are rated up to 400 amps continuous current.
06:00Whereas the VERSO LT is rated for 100 amps.
06:05Next, the last hour value provides the average load over the last 60 minutes.
06:09If the rec closure is being installed in a new location or additional load is being added to
06:14the line, this value may be reset to measure fresh load data.
06:18Finally, the peak value is the peak current scene during a one minute interval of the last
06:24hour. As with the last hour value, this value can be
06:27reset at any time in order to clear any previously measured data points in the versa
06:33two and XCU I an hourly demand log is also display which shows the peak and average hourly
06:39R MS currents when loaded, the demand log values are shown and are also graphed to
06:45visually display the R MS load profile over the period of time loaded.
06:50The event tab in each of the VERSO UIs is primarily used to display rec closure over
06:55current events, which includes identifying the shot number type of event control response time
07:01max over current amperage and curve name.
07:04However, dependent on reclosing type, what is displayed slightly differs,
07:09for example, in the versa, C one and LTU I an hourly demand log is displayed in this tab and
07:15shows the peak and average hourly R MS currents as with the VT two and XCU I when loaded,
07:22the demand log is graphed to visually display the R MS load profile over the past month.
07:28In the VERS two and XCU I no demand log is shown under the events tab.
07:33However, the user may select a particular event in the event log and see oscillatory for the
07:39program number of pre trip and post trip cycles along with that event specific to the versa two
07:45and X closure U I is a device log tab. This includes all the control commands that are
07:51sent in the firmware to for example, open or close the bottle update GPS detect default
07:57clear a fault reach low battery mode, et cetera.
08:01Also specific to the versa two and X eu I is the commands tab.
08:06This tab provides six commands and associated radio buttons to change the state of the rec
08:10closure. For example, a user may flash the led beacon to
08:15identify the device place the rec closure in hotline tag or non relo mode,
08:20open the bottle, close the bottle or send the device to lockout,
08:24which includes dropping the yellow handle.
08:27If the user places the rec closure in HLT mode, the associated pattern beacon will flash to
08:32indicate the rec closure is in that mode.
08:35Additionally, it is important to note that if the rec closure is sent to lockout and the
08:39yellow handle drops, the unit cannot be closed via the close command through the U I.
08:44This requires a manual reset by the user on any tab of the U I.
08:50The user can view the user name, the firmware revision on the control board,
08:54the radio type or serial used to communicate with the rec closure and the hardware revision.
08:59Additionally, the rec closure UTC time and the serial number of the rec closure is displayed
09:05also provided in the versa U I are additional indicators to allow the user to know in which
09:11state the reclosing is along the bottom edge of the U I top middle of the VT one U I in the
09:17versa two and X eu I, there are four buttons that illuminate if the rec closure is currently
09:22in that state, these include the contacts being open, green or close red.
09:28And if the rec closure is in HLT orange mode or NR red mode with the versa
09:35two and X EU I A user is provided additional visibility in the advanced status menu on the
09:41state of the battery under rec closure status as well as the current GPS coordinates.
09:45And number of satellites under GPS status.
09:49Finally, in any versa, ui a user can generate a report, generate report in the upper right hand
09:56of the window. The report provides a detailed summary of all
09:59rec closure settings, rec closure status, event logs, device logs,
10:04audit logs, demand, logs, firmware, revision and more,
10:08this report may be generated on any PC ipad or iphone app.
10:13And the information included may be tailored by the user through a pop up window which appears
10:17when the generate report button is selected.
Using Hubbell Power System’s Versa-Tech Programmer, the Versa-Tech recloser is as simple to program as it is to install. With a Windows-based computer or an iPad, the Versa-tech can be programmed prior to installation or after installation at any time. An instruction manual included with each recloser provides step-by-step instructions on how to connect to and program the various settings specific to each type of Versa-Tech recloser.