Transcript
00:09This video looks at the refinishing and repair of chance epoxy glass poles.
00:14First, let's look at the sanding and refinishing of an epoxy glass pole,
00:19inspect the pole for any damages such as impact areas that may affect the mechanical or
00:24electrical properties of the tool.
00:27If only sanding is required, use the abrasive pad emery cloth and moisture eater.
00:32Two cleaner solvent to remove the old finish.
00:35Once that is done, wipe the area down with moisture eater.
00:38Two to remove any contaminants, mix up the two part gloss restorer
00:45or pigmented orange finishing paint and pour into a squeeze bottle.
00:49Use a foam brush to apply a uniform coat on the pole, let dry for
00:5624 hours. And if additional coat is required,
00:58apply a second coat after the first is cured.
01:04Now, let's look at the patching of an epoxy glas pole except the epoxy glass bond patching
01:11kit per the instructions
01:18apply liberally in the damaged area.
01:22Smooth out using cellophane tape around the patch area to help let dry for 24 hours.
01:29Remove the tape and send the area smooth, reapply the gloss restorer to the patched area
01:35to seal the pole surface let drive for 24 hours.
01:41Next. Let's look at the installation of a universal
01:44head cut off the damaged universal fitting measure the depth of the universal fal
01:51sand. The pole from the end down the pole, the depth
01:53of the pal with sandpaper or emery cloth, wipe sanded area with
02:00moisture eat or two cleaner solvent to remove any foreign material.
02:04Mix up the epoxy Glas bond patching kit per the instructions.
02:09Applaud the epoxy bond inside of Farrell in the Senate area of the pole.
02:15Install Farrell to correct depth. Be sure.
02:17It's fully seated drill. 1 1964 hole through one side of the
02:24Farrel at the midpoint.
02:26Install spiral drop pin, wipe off any excessive epoxy that may have
02:33squeezed out of the feral.
02:39Last, let's look at plugging the pole and the installation of a butt swivel,
02:45cut the damaged end of the stick off to the desired length at cut end,
02:49remove the foam to a dimension of four inches.
02:52Use epoxy Glas plug kit, mix up epoxy per the instructions
03:00fixture the pole in vertically and pour the plug mix into the top of the pole let cure for
03:0424 hours sand the pole from the end down to the depth of the feral measurement with sandpaper
03:10or emery cloth, wipe sanded area with moisture eat or two cleaner solvent to remove any
03:15foreign material. Mix up the epoxy bond kit,
03:19individual packet or quart container for the instructions coat the inside of the butt swivel
03:24feral with epoxy and also the scented area of the pole,
03:28install the butt swivel onto the pole. Be sure it's fully seated onto the pole.
03:33Wipe off any excessive epoxy that may have squeezed out of the fre and smooth epoxy out
03:37around the bottom of the fre using a 1764 inch drill bit drill holes in the center of the four
03:43bosses, do not drill completely through the feral drill to a depth of about half an inch.
03:49After drilling the four holes, install the four flu to drive pins.
03:52Be sure that the pins are flush with the feral and do not protrude above the feral.
03:57Set the tool aside and let dry for 24 hours.
04:01All repairs and refinishing should be followed by electrical testing of the tool before
04:04putting the tool back into service.
04:07For more information, please call customer service or visit hubble.com.
Refinishing and repair of Chance Epoxiglas Poles.