HUBBELL WIRING DEVICE-KELLEMS

Installation

Dimmer Switch can be for a single pole setup, or for use with 3- and 4- way configurations when using multiple Dimmer Switches.

In 3- and 4- way configurations, traveler wire should not be used.

A neutral wire must be present in each gang box.

Installing Dimmer Switch - Single Pole
Installing Dimmer Switch: 3- and 4-way
How to Find the Primary Switch
Pairing Switches Together
Dimmer Switch Setup on iOS 11 and Later
Dimmer Switch Setup on Android
Dimmer Switch Setup on Both iOS & Android
Dimmer Switch, In the Box

Using Your Dimmer Switch

Before replacing your bulb, pull out the air gap switch between the bottom two buttons to cut power to the bulb.

Dimmable feature requires a dimmable bulb.

The Dimmer Switch night light is controlled independently from the switch.

If you're experiencing bulb flicker, be sure to set your dim levels.

Dimmer Switch Button Controls
What are Dim Levels
Setting Bulb Dim Levels
Changing the Bulb with Dimmer Switch
Downloading New Firmware
Dimmer Switch Safe Usage Guidelines

Problem Solving

Rebooting the device can quickly resolve many issues.

A blinking orange LED indicates the product is no longer connected to the Wi-Fi network or internet.

Be sure to turn on iCloud Keychain to avoid any HomeKit errors.

Rebooting Products
Resetting Dimmer Switch
Troubleshooting 3- and 4-way Pairing
Dimmer Switch, Couldn't Add Accessory on iOS
Accessory Isn't Compatible with Router
Dimmer Switch, Wi-Fi Network Not Found
Changing Wi-Fi Networks
Dimmer Switch LED Status Summary
iCloud is Synchronizing
Dimmer Switch, No Products Available on iOS
Dimmer Switch is Unavailable on iOS

Compatibility

Wi-Fi And Network Setup
3-, 4-Way Configurations
Mobile Device Compatibility
Power Ratings and Product Specifications
Remote Access
Apple Home Hub Remote Access
iDevices Connected App

Remote Access Requirements

Use Instinct remotely with the Amazon Alexa app.

All other produts work remotely through the iDevices Connected App.

Remote Access
Apple Home Hub Remote Access

Wi-Fi And Network Compatibility

An adequate Wi-Fi network is required to sufficiently operate connected products.

Consider including additional access points for buildings with concrete walls and ceilings, as those can block signal.

Be sure Airtime fairness or Airtime Quality settings are disabled on your router.

Products should be set up on a 2.4GHz network band.

Network Requirements
Planning Your Network
Changing Wi-Fi Networks

Need Further Assistance? We're Here To Help.

Our Customer Experience Team is available Mon - Fri 9am - 5:30pm EST